Dear all,
My codebase is DM365IPNC_V2.6. The default kernel config uses Preemptible Kernel (Low-Latency Desktop) mode, but I want to change it to Complete Preemption(Real-Time) mode. After this change, I will encounter the encode error. As I know the whole SDK is based on preemptible kernel mode to develop, so I change this setting will affect the priority of process. I think that is the main reason to cause the encode error. Is my view right? If I want to resolve this issue, I think need to base on Complete Preemption(Real-Time) mode to rally the SDK. Can anyone help me to confirm that? Thanks in advance.
B.R.
OC