This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3894: eMMC Support, USB OTG, SERDES, PCIe Clock, Reference Design?

Other Parts Discussed in Thread: AM3894

Questions from customer:

1) Can I connect eMMC FLASH storage to the AM3894 ...I already have an SD card connected and NAND FLASH connected but not sure how to add eMMC say 32GB to the design

2) How can I use one of the two USB ports as device (Client) or better as OTG? 

3) I want to use the AM3894 to program ALTER's FPGA and which SERDES can use for the serial I/F for this?

4) I want to connect AM3894 to PCI switch - but not sure about the clocks and who generates them...any same schematic where the AM3894 is connect to another PCIe

5) We  want to connect the video input/output buses to ALTERA FPGA...but I can only see parallel buses  - is there a way to get the Diff LVDS to input/output video?

6) Having issues in down loading AM3894 REF manual? are there any other schematic then  one from Spectrum Digital?

8) What port can I use for SPDIF ~ any example schematics? for optical but coax is OK too