This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VPSS issues on dm814x

I am working on the dm814x processor, and using EZSDK-evm_5_03_01_15.

I was able to load the VPSS m3-firmware and tough i can't  ' $ cat pic.raw > /dev/fb0 '  and see the picture stays there, i do able to run Qt application and these apps works fine.

Now, there are two problems that occur:

1) When loading the VPSS firmware, the tty3 is stuck and i have to continue via Telnel in order to use the linux's terminal.

2) When i want to use the DSP and load a firwmare to it, i have to turn off the VPSS, or counterwise, in order to use VPSS so i have not to load firmware to the DSP.

Any guideline how to solve these two issues?