hello:
I use the c6455 with NDK, and c6455 run as server, when I run my project, I ping the IP, it is OK, and then I telnet the server port, it is not OK! Bind and listen all are OK!
I don't know why ! I need help !
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello:
I use the c6455 with NDK, and c6455 run as server, when I run my project, I ping the IP, it is OK, and then I telnet the server port, it is not OK! Bind and listen all are OK!
I don't know why ! I need help !
Thanks!
Hi si cheng,
Which version of the NDK are you using? Which version of BIOS?
Are you running one of the NDK examples? If so, which one are you trying to run?
Steve