This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Stand Alone Program ezdsp5515/ezdps5505



Hi,

I would create a stand alone program in ezdsp5515. I have used the examples programs included in C5000 Teaching ROM based on ezDSP5505/ ezDSP5515. Everthing is OK when the program run in debugging mode. But whem the program is flashed, It does not work. I know the flashing process is OK. I have flashed Audio Program, and also the demo program Spectrum digital provides. I think the problem is relate to the initialization the GEL file does automatically in debugging mode.

Does anyone has flashed any of the program included in C5000 teaching ROM in the ez5505/5515. ?

Another option I have also tried is modifying the Audio Demo program. This file contain the necessary initialization in the program. I have stored in flash and the application run OK, but this way I can not use the function include in the teaching ROM. 

Thank you