Other Parts Discussed in Thread: AM3703
We purchased LI-3M02.
It is due to connect with the trial production board of our company which
carries AM3703 .
There is a question about the sample software of LI-3M02.
Sample software carries out the following operation, when connecting with TI
EVM, Inc.
■Camera Loopback Example
Camera example application demonstrates streaming of YUV 4:2:2 parallel data
from Leopard Imaging LI-3M02 daughter card with MT9T111 sensor on AM37x EVM.
Here, driver allocated buffers are used to capture data from the sensor and display
to any active display device (LCD/DVI/TV) in VGA resolution (640x480).
However, when connecting with the trial production board of our company, I would
like to move a camera first of all.
It is because LCD differs from TI EVM, Inc., so operation will become
complicated if it corresponds to a LCD display.
I would like to consider it as the operation which saves in a memory the data
which carried out camera acquisition.I would like to, check only a motion of the
camera portion in our board first of all.
Is such how to move possible at sample software?