Other Parts Discussed in Thread: OMAPL138, CCSTUDIO
Hi,
I am using OMAPL138, CCS 5.1.1, Bios 6.33.03.33, PSP 03.00.01.00, xdc 3.23.01.43.
I want to run my DSP and ARM at 405MHz. I changed PLL settings in ARM for all SYSCLK frequencies.
Now I have created a custom RTSC platform and set Clock frequency to 405MHz.
With this both ARM and DSP are running at 405MHz.
I am using PSP drivers and I see that SYSCLK frequencies are still at default 300MHz (based on the clock for some peripherals like UART).
Earlier I have changed SYSCLK frequencies in PSP/CSLR and compiled PSP platform.
Is there any way to do this without PSP/CSLR changes?
thanks, Durga