This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C66X PCIe boot example



Dear all:

I try to run the example code about PCIe boot in    \ti\mcsdk_2_00_04_16\tools\boot_loader\examples\pcie

The first step is

       Import the project from tools\boot_loader\examples\pcie\pcieboot_ddrinit\evmc66xxl in CCSv5 •

The second step is

    Clean and re-build the project

But the project don't have any " .cfg" file so that I can't build this project~

Has anyone could help me?Thanks~

Best Regards,

W.T.

 

 

 

 

 

 

 

  • This project does not need BIOS, so you don't have cfg file. They have the cmd file that defines the sections. Try the latest MCSDK 2.0.7. This is more updated and stable.

    Thanks,

    Arun.

  • Dear Arun:

    Thanks for your reply.I still have one problem about programming "IBL".

    In the  \mcsdk_2_00_07_19\tools\boot_loader\examples\pcie\docs\README ---> page15   it mentions that:

    "please update IBL with the latest from MCSDK by following the step 1--- 

    Programming "IBL" on the EEPROM at bus address 0x51 in tools\boot_loader\ibl\doc\evmc66xx-instructions.txt."

    Could you tell me how to execute"Programming "IBL" on the EEPROM at bus address 0x51"?

    Thanks a lot

    Best Regards,

    W.T.

     

  • WT,

    The easy way for installing the new IBL, is to run program_EVM script in the tools\program_evm.

    thanks,

    arun.