This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IPV6 Support

Dear all,

Our NDK supports the following software

The NDK includes:

 

Core TCP/IP protocol stack: Dual-mode IPv6/IPv4 stack in both source and binary only including VLAN packet priority marking, TCP, UDP, ICMP, IGMP, IP, and ARP Network applications: HTTP, TELNET, TFTP, DNS, DHCP (IPv4 only) in both source and binary form Application Programming interfaces: BSD Sockets, including support for raw Ethernet Device drivers: Pre-tested device drivers in source and binary form for the on-chip EMACs of supported DSPs.

 

I need to know when we will have full support to IPv6 to Network applications: HTTP, Telnet, TFTP, DNS, DHCP

 

TKs and Rgds,
Letice