Hello,
I could use some advice on how to compile this library in CCSv5. The instructions I have found in the directory are vague and limited to makefiles and CCsv4. Also, what is the best way to link this into an RTSC project? Can I put it into the config file some how?
The below instructions don't work and build a .out file, not a library.
The following tools are required to build IMGLIB using CCS (links provided). Download and install all tools to a single local (C:)
directory, for example, c:\Program Files\Texas Instruments
.
- Note:
- A "My.TI" account is required for download and can be registered at my.ti.com
The IMGLIB may be compiled with CCS following the procedure below:
- Open CCS
- Import the IMGLIB makefilebased project
- Open the Projectmenu
- Select Import Existing Eclipse Project
- Import from the IMGLIB
/lib directory
- Modify install paths and settings in makefileif necessary
- Within CCS, open the makefile from the ProjectTAB
- Check the CGT path: C6X_GEN_INSTALL_DIR
- Check the CGT version: CCSCGTVER
- Check the CCS path: CCS_INSTALL_DIR
- Check the IMGLIB path: IMGLIB_INSTALL_DIR
- Build the project
- Select Rebuild Active Project from Project menu
- Note:
- If the RMDIR utility in the makefile is not recognized, you may need to redefine it for a local utility.
And these library instructions don't work either:
Linking IMGLIB
The path to the IMGLIB libraries must be provided to the linker via the -l directive. See Library Directory for IMGLIB library details. |