This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VLIB and the DM8148



Has anyone successfully integrated and used one the VLIB example projects with the TI DM8148 EVM? 
When I tried to import an example project from the VLIB installation directory CCS5.1 for Linux failed to import the project successfully complaining that a BIOS was unavailable which is the case and although the BIOS  was installed CCS doesn't seem to realize that or be capable of adding it to the RTSC.  See attachement for CCS5.1 for Linux full installation configuration defaults. 

4478.Doc1.doc