Dear all,
I am using Technexion's TAO3530 (OMAP3530 processor) with Wince6.0 R3. The BSP is provided by Technexion as it is without support, I think it is because they probably dont't do the video driver part in the BSP.
This board is configured for 720p but for Philips 55PFL6606 and many Samsung TVs I tested also cannot display. So far I have tested it works on Panasonic, LG, Sharp, Haier TVs.
The transceiver chip used is TI's TFP410.
I have doubt is this a video registers value settings? Or transceiver chip problem? Or something else related to the transceiver chip.
I am trying very hard to study and understand the hardware as well as Wince driver so that I can solve this problem.
Can somebody please give some pointers and suggestion to help me resolve this issue. I could provide the schematic, video driver sorce code file.