Hi,
I am using the DM368 and have set LBRmaxpicsize to 10 in order to keep the frames roughly the same size. Normally this works fairly well, but I notice that the size of the IDR can spike quite a bit above the size specified by BitRate/FrameRate. I have tried using rcAlgo of 0 and 5, and have set rcQMin=0, rcQMinI=0, rcQMax=51 and rcQMaxI=51 in order to let the encoder use the full range of quantization (as far as I know).
Is there any other method of controlling the frame size that will allow me to always keep it within the BitRate/FrameRate limit? If it would help I can gather some print outs of the frame sizes I am seeing, and can show any other encoder parameters necessary.
Thanks,
Chris