Hi all
I have a mistral version DM8148 evm board and a customized board with 2 tvp5158 on it.
I have successfully ported the DVRRDK_02.00.00.23 and can run DM814x demo.
I have test the capture,h264 encode,h264 decode,hdmi display and standard display.
all works well excep one thing.
I see a lot of record file with name VBITS_DATA_x.bin and VBITS_DATA_x.bin.mv but where
is the jpeg(mjpeg file)?
My usecase is VSYS_USECASE_MULTICHN_PROGRESSIVE_VCAP_VDIS_VENC_VDEC_8CH.
so I think the mjpeg file maybe VBITS_DATA_16(or above).bin , but the file size is 0.