This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Syslink Error with Vc3 Demo



Hi,

    I am trying to run the VC3 demo from the SDK 5.03.01.15 released last December. I followed all the steps to to generate executables for M3 and host. I copied the .xem3 from vc folder..

   The moment I run the "vc3_a8host_debug.xv5T", I am getting the following error continiouisly...

Assertion at Line no: 430 in /work/ti_sdk_03_01_15/component-sources/syslink_2_0 0_05_85/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/ip c/hlos/knl/Linux/SharedRegionDrv.c: (status >= 0) : failed

Assertion at Line no: 430 in /work/ti_sdk_03_01_15/component-sources/syslink_2_0 0_05_85/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/ip c/hlos/knl/Linux/SharedRegionDrv.c: (status >= 0) : failed

Any Idea, Why this error is coming? I built the firmloader and updated as well...

Thanks

 Bose