This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Interfacing ADS8556 with OMAP-L138

Other Parts Discussed in Thread: OMAP-L138, OMAPL138, ADS8556

Hello,

I am trying to interfacing ADS8556EVM  with Zoom™ OMAP-L138 eXperimenter Kit. In order to do this, I used an SPI0 interface on OMAP-L138. This work exellent, but in our project I use Ethernet, and I could not use SP0 at the same time. Further I am trying to use SPI1 interface. This is work, but  not properly, because I have an old version of OMAP-L138 eXperimenter Kit, and the output buffer, which connect to SPI flash, always driving SPI1_SOMI on the bus. Further I am trying McBSP1 interface to interfacing ADS with OMAP, but CLKSTP mode is not supported on OMAP-L138. And, as I understand, I can not use it in SPI master mode ? 

In this situation, I see the only way - connecting ADS8556EVM with OMAP-L138 eXperimenter Kit  via universal parallel port. Can anyone advise me how to do it? 

I am using CCS v5.1, SYS/BIOS 6.33.04.39, BSL by LogicPD for SPI interface, and BIOSPSP for McBSP interface.

Thanks,

Ilya