This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

how to set memory layout of c6a816x while doing codec engine project?



hello,experts

I'm using codec engine example of videnc_copy to do my own video encoding work.

Now I have completed the  codec,server and app  source code. So I wonder where to config my DSP memory layout  like in  file " link.cmd " of  CCS project .I have read the "codec engine aplication developer/server integrator/algorithm creator  user guide" but find no answer.

for example  in a c6a816x.cmd file,there are some memory layout like below:


-heap 0x400000
-stack 0x2000

MEMORY
{
DSPL2 o = 0x00800000 l = 0x00040000 /* 256kB DSP L2 RAM */
DSPL1P o = 0x00E00000 l = 0x00008000 /* 32kB DSP L1 Program Cache/RAM */
DSPL1D o = 0x00F00000 l = 0x00008000 /* 32kB DSP L1 Data Cache/RAM */
L3OCMC0 o = 0x40300000 l = 0x00040000 /* 256kB L3 OCMC SRAM */
L3OCMC1 o = 0x40400000 l = 0x00040000 /* 256kB L3 OCMC SRAM */
SHDSPL2 o = 0x40800000 l = 0x00040000 /* 256kB Shared DSP L2 RAM */
SHDSPL1P o = 0x40E00000 l = 0x00008000 /* 32kB Shared DSP L1 Program Cache/RAM */
SHDSPL1D o = 0x40F00000 l = 0x00008000 /* 32kB Shared DSP L1 Data Cache/RAM */
DDR0 o = 0x80000000 l = 0x40000000 /* 1GB external DDR Bank 0 */
DDR1 o = 0xC0000000 l = 0x40000000 /* 1GB external DDR Bank 1 */
}

SECTIONS
{
.text > DDR0
.stack > DDR0
.bss > DDR0
.cio > DDR0
.const > DDR0
.data > DDR0
.switch > DDR0
.sysmem > DDR0
.far > DDR0
.args > DDR0
.ppinfo > DDR0
.ppdata > DDR0

/* TI-ABI or COFF sections */
.pinit > DDR0
.cinit > DDR0

/* EABI sections */
.binit > DDR0
.init_array > DDR0
.neardata > DDR0
.fardata > DDR0
.rodata > DDR0
.c6xabi.exidx > DDR0
.c6xabi.extab > DDR0
}

I just want to know how to do this work in codec engine examples.Thank you very much!