Hi,
I have tried the HUA application successfully using emulator cable outside the computer. But when I assembled the board with AMC TO PCIe adapter and pluged into the PCI socket on motherboard, the system can not find the board.
Firstly in no boot mode, I updated the MCSDK of the board, which had been connected with AMC PCIe adapter, as the procedures in 10.3 at http://processors.wiki.ti.com/index.php/BIOS_MCSDK_2.0_User_Guide. There was no errors besides the errors can not find the .c source code files.
Secondly, I pluged the board into an open PCI socket on the motherboard. Set the board at PCIe boot mode.
Thirdly, turn on the computer power. At command line, I can not find the mutimedia controller like the discription at TMDXEVMPCI FAQs.pdf.
I have tried two computers and repeated the whole process several times. I used ubantu 11.04. CCS5.1 and MCSDK2.0.7.19.
Could you please help me analyze what the problem is?