This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Touchscreen doesn't work! at OMAP3530 EVM board.

Other Parts Discussed in Thread: MIDAS, OMAP3530, SYSCONFIG, ADS7846

I try MIDAS v2.0 following web site http://processors.wiki.ti.com/index.php/MIDAS_Ultrasound_v2.0_Demo

I think that I succeeded compile in everything except touch screen.

I try Touchscreen Setup follow web site blow.

Touchscreen Setup

MIDAS utilizes the tslib library for touchscreen support on the OMAP3530 EVM. This section will guide you through setting up tslib. 

1. Install required packages on host

host $ sudo apt-get install autogen autoconf libtool

2. For cross-compiling, define environment variables in ~/.bashrc on host as:

export CC=/home/<username>/arm-2009q1/bin/arm-none-linux-gnueabi-gcc export CXX=/home/<username/arm-2009q1/bin/arm-none-linux-gnueabi-g++ export CONFIG_SITE=omap3evm.autogen 

3. Download the source files for tslib from here and save it at ~

4. Untar the source

host $ cd ~host $ tar xjf tslib-1.0.tar.bz2

5. Configure tslib

host $ cd ~/tslib-1.0 host $ ./autogen.sh host $ ./configure --prefix=/home/<username>/workdir/filesys --host=arm-linux-gnu

6. Comment the line ‘AC_FUNC_MALLOC’ in ~/tslib-1.0/configure.ac

7. Comment ‘#define malloc rpl_malloc’ in ~/tslib-1.0/config.h if it exists

8. Build and install tslib

host $ make host $ make install

9. Edit ~/workdir/filesys/etc/ts.conf to use linux layer event interface by uncommenting ‘module_raw input’

10. Modify the device’s startup script to export the required touchscreen related environment variables.

    Add these lines to the file ~/development/workdir/filesys/etc/profile:

export QWS_MOUSE_PROTO='Tslib:/dev/input/event1' export TSLIB_CALIBFILE='/etc/pointercal' export TSLIB_CONFFILE='/etc/ts.conf' export TSLIB_CONSOLEDEVICE='none' export TSLIB_FBDEVICE='/dev/fb0' export TSLIB_PLUGINDIR='/lib/ts' export TSLIB_TSDEVICE='/dev/input/event1'

11. Remember to run ‘ts_calibrate’ on the target the first time you start the board, to calibrate the touch screen.

I inputed command ts_calibrate and I get some message blow.


omap3evm login: root

root@omap3evm:~# ts_calibrate
No raw modules loaded.
ts_config: Success
root@omap3evm:~#

root@omap3evm:~# <4>omap-dss: Could not find exact pixel clock. Requested 25188 kHz, got 25187 kHz
omap-dss: Could not find exact pixel clock. Requested 25188 kHz, got 25187 kHz

                


I'm looking for "Could not find exacpt pixel clock" at google and e2e.ti.com.

I found a  TI member as same error message. ( http://e2e.ti.com/support/dsp/omap_applications_processors/f/447/t/94126.aspx )


But I didn't get enough answer.

So I try that as indicated.

First, I input command ls -la /dev/input.


root@omap3evm:~#

root@omap3evm:~# ls -la /dev/input/

drwxr-xr-x    2 root     root          100 Jan  1  1970 .

drwxr-xr-x   10 root     root         3060 Sep 11 16:17 ..

crw-r-----    1 root     root      13,  64 Jan  1  1970 event0

crw-r-----    1 root     root      13,  65 Jan  1  1970 event1

lrwxrwxrwx    1 root     root            6 Jan  1  1970 touchscreen0 -> event1

root@omap3evm:~#

root@omap3evm:~#


Second, I input command cat /proc/bus/input/devices


root@omap3evm:~#

root@omap3evm:~# cat /proc/bus/input/devices

I: Bus=0019 Vendor=0001 Product=0001 Version=0003

N: Name="omap_twl4030keypad"

P: Phys=omap_twl4030keypad/input0

S: Sysfs=/class/input/input0

U: Uniq=

H: Handlers=kbd event0

B: EV=100003

B: KEY=1680 0 70032 53840000

I: Bus=0000 Vendor=0000 Product=0000 Version=0000

N: Name="ADS784x Touchscreen"

P: Phys=spi1.0/input0

S: Sysfs=/class/input/input1

U: Uniq=

H: Handlers=event1

B: EV=b

B: KEY=400 0 0 0 0 0 0 0 0 0 0

B: ABS=1000003

root@omap3evm:~#    

3th, I input command cat /dev/input/event0 & 1 and touch screen.

          root@omap3evm:~# cat /dev/input/event0 

There is no response when I touched the screen.

I input command cat /dev/input/event1 & touch screen.

There is something reactions.


root@omap3evm:~# cat /dev/input/event1 

}z▒JǗ~z▒J▒J~z▒J▒~z▒Jz▒J▒:z▒Jz▒J▒:

z▒J▒:z▒J▒z▒Jz▒J▒d

▒J▒dz▒J▒dPuTTYPuTTYPuTTYPuTTYPuTTYPuTTYPuTTYPuTTYPuTTz▒Jz▒J▒▒

z▒J▒▒z▒J▒z▒J]

z▒J]z▒Jz▒J>▒z▒J>▒▒     z▒J>▒z▒J>z▒J▒z▒J▒▒      z▒J▒z▒Jz▒J▒9z▒J:▒       z▒Jz▒J▒yz▒J▒yv  z▒J▒yz▒J▒z▒J▒▒z▒JΚh  z▒JΚz▒Jz▒J▒▒z▒J▒▒>      z▒J▒z▒Jz▒J6m            z▒J6z▒Jz▒Jgz▒Jz▒Jgz▒Jz▒J▒

        z▒J▒

       z▒J▒

        z▒J▒

       z▒J▒▒    z▒J▒▒  z▒J▒▒    z▒J▒▒  z▒J▒     z▒J▒   z▒J/▒

4th, I input command ls -la /lib/ts


root@omap3evm:~#

root@omap3evm:~# ls -la /lib/ts/

drwxr-xr-x    2 1000     1000         4096 Apr 27  2012 .

drwxr-xr-x    6 1000     root         4096 Apr 27  2012 ..

-rwxr-xr-x    1 1000     1000          944 Apr 27  2012 arctic2.la

-rwxr-xr-x    1 1000     1000         5631 Apr 27  2012 arctic2.so

-rwxr-xr-x    1 1000     1000          938 Apr 27  2012 collie.la

-rwxr-xr-x    1 1000     1000        10498 Apr 27  2012 collie.so

-rwxr-xr-x    1 1000     1000          932 Apr 27  2012 corgi.la

-rwxr-xr-x    1 1000     1000         5597 Apr 27  2012 corgi.so

-rwxr-xr-x    1 1000     1000          950 Apr 27  2012 dejitter.la

-rwxr-xr-x    1 1000     1000         6658 Apr 27  2012 dejitter.so

-rwxr-xr-x    1 1000     1000          932 Apr 27  2012 h3600.la

-rwxr-xr-x    1 1000     1000         5625 Apr 27  2012 h3600.so

-rwxr-xr-x    1 1000     1000          932 Apr 27  2012 input.la

-rwxr-xr-x    1 1000     1000         7163 Apr 27  2012 input.so

-rwxr-xr-x    1 1000     1000          938 Apr 27  2012 linear.la

-rwxr-xr-x    1 1000     1000         8810 Apr 27  2012 linear.so

-rwxr-xr-x    1 1000     1000          974 Apr 27  2012 linear_h2200.la

-rwxr-xr-x    1 1000     1000         6368 Apr 27  2012 linear_h2200.so

-rwxr-xr-x    1 1000     1000          932 Apr 27  2012 mk712.la

-rwxr-xr-x    1 1000     1000         5629 Apr 27  2012 mk712.so

-rwxr-xr-x    1 1000     1000          938 Apr 27  2012 pthres.la

-rwxr-xr-x    1 1000     1000         6479 Apr 27  2012 pthres.so

-rwxr-xr-x    1 1000     1000          944 Apr 27  2012 ucb1x00.la

-rwxr-xr-x    1 1000     1000         5535 Apr 27  2012 ucb1x00.so

-rwxr-xr-x    1 1000     1000          950 Apr 27  2012 variance.la

-rwxr-xr-x    1 1000     1000         6545 Apr 27  2012 variance.so

root@omap3evm:~#

5th, I input command  cat /etc/ts.conf


root@omap3evm:~#

root@omap3evm:~# cat /etc/ts.conf

# Uncomment if you wish to use the linux input layer event interface

# module_raw input

# Uncomment if you're using a Sharp Zaurus SL-5500/SL-5000d

# module_raw collie

# Uncomment if you're using a Sharp Zaurus SL-C700/C750/C760/C860

# module_raw corgi

# Uncomment if you're using a device with a UCB1200/1300/1400 TS interface

# module_raw ucb1x00

# Uncomment if you're using an HP iPaq h3600 or similar

# module_raw h3600

# Uncomment if you're using a Hitachi Webpad

# module_raw mk712

# Uncomment if you're using an IBM Arctic II

# module_raw arctic2

module pthres pmin=1

module variance delta=30

module dejitter delta=100

module linear

root@omap3evm:~#

What is the problem?

Please tell me the solution.


Additional noted items.

root@omap3evm:~# dmesg

Linux version 2.6.29-rc3-omap1 (won@ubuntu) (gcc version 4.2.3 (Sourcery G++ Lite 2008q1-126)) #6 Thu Apr 26 19:45:05 KST 2012

CPU: ARMv7 Processor [411fc083] revision 3 (ARMv7), cr=10c5387f

CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache

Machine: OMAP3 EVM

Memory policy: ECC disabled, Data cache writeback

On node 0 totalpages: 58112

free_area_init_node: node 0, pgdat c0440c24, node_mem_map c0465000

  Normal zone: 512 pages used for memmap

  Normal zone: 0 pages reserved

  Normal zone: 57600 pages, LIFO batch:15

OMAP3530 ES3.1 (full speed SGX, IVA2)

SRAM: Mapped pa 0x40200000 to va 0xd7000000 size: 0x100000

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 57600

Kernel command line: console=ttyS0,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nfsroot=192.168.1.100:/home/won/workdir/filesys,nolock mem=99M@0x80000000 mem=128M@0x88000000 mpurate=600 omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y

Clocking rate (Crystal/DPLL/MPU core): 26.0/332/500 MHz

IVA2 clocking rate: 360 MHz

Reprogramming SDRC

GPMC revision 5.0

IRQ: Found an INTC at 0xd8200000 (revision 4.0) with 96 interrupts

Total of 96 interrupts on 1 active controller

OMAP34xx GPIO hardware version 2.5

PID hash table entries: 1024 (order: 10, 4096 bytes)

OMAP clockevent source: GPTIMER1 at 32768 Hz

Console: colour dummy device 80x30

Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)

Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)

Memory: 99MB 128MB = 227MB total

Memory: 225664KB available (3928K code, 370K data, 156K init)

Calibrating delay loop... 499.92 BogoMIPS (lpj=1949696)

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

net_namespace: 520 bytes

NET: Registered protocol family 16

MUX: setup AF26_34XX_GPIO0 (0xd80021e0): 0x011c -> 0x0118

MUX: setup L8_34XX_GPIO63 (0xd80020ce): 0x0118 -> 0x0004

MUX: setup AF9_34XX_GPIO22 (0xd80025ec): 0x0100 -> 0x011c

MUX: setup U3_34XX_GPIO61 (0xd80020c8): 0x0118 -> 0x011c

MUX: setup AH14_34XX_GPIO21 (0xd80025ea): 0x0100 -> 0x011c

MUX: setup AA10_3430_USB2HS_PHY_STP (0xd80025f2): 0x0100 -> 0x0003

MUX: setup AA8_3430_USB2HS_PHY_CLK (0xd80025f0): 0x0100 -> 0x0003

MUX: setup AA9_3430_USB2HS_PHY_DIR (0xd80025f4): 0x0100 -> 0x010b

MUX: setup AB11_3430_USB2HS_PHY_NXT (0xd80025f6): 0x0100 -> 0x010b

MUX: setup AB10_3430_USB2HS_PHY_D0 (0xd80025f8): 0x0100 -> 0x010b

MUX: setup AB9_3430_USB2HS_PHY_D1 (0xd80025fa): 0x0100 -> 0x010b

MUX: setup W3_3430_USB2HS_PHY_D2 (0xd80021d4): 0x0108 -> 0x010b

MUX: setup T4_3430_USB2HS_PHY_D3 (0xd80021de): 0x0108 -> 0x010b

MUX: setup T3_3430_USB2HS_PHY_D4 (0xd80021d8): 0x0100 -> 0x010b

MUX: setup R3_3430_USB2HS_PHY_D5 (0xd80021da): 0x0100 -> 0x010b

MUX: setup R4_3430_USB2HS_PHY_D6 (0xd80021dc): 0x0108 -> 0x010b

MUX: setup T2_3430_USB2HS_PHY_D7 (0xd80021d6): 0x0100 -> 0x010b

twl4030: client 1 is not initialized

twl4030: client 1 is not initialized

MUX: setup AA21_34XX_GPIO157 (0xd800218e): 0x0018 -> 0x011c

MUX: setup C23_34XX_GPIO98 (0xd8002114): 0x0004 -> 0x011c

omap3evmdc: Driver registration complete

Switched to new clocking rate (Crystal/Core/MPU): 26.0/332/600 MHz

IVA2 clocking rate: 430 MHz

Calibrating delay loop... 597.64 BogoMIPS (lpj=2334720)

OMAP DMA hardware revision 4.0

USB: No board-specific platform config found

OMAP DSS rev 2.0

OMAP DISPC rev 3.0

OMAP VENC rev 2

OMAP DSI rev 1.0

bio: create slab <bio-0> at 0

i2c_omap i2c_omap.1: bus 1 rev3.12 at 2600 kHz

twl4030: PIH (irq 7) chaining IRQs 368..375

twl4030: power (irq 373) chaining IRQs 376..383

twl4030: gpio (irq 368) chaining IRQs 384..401

i2c_omap i2c_omap.2: bus 2 rev3.12 at 400 kHz

i2c_omap i2c_omap.3: bus 3 rev3.12 at 400 kHz

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

musb_hdrc: version 6.0, musb-dma, host, debug=0

HS USB OTG: revision 0x33, sysconfig 0x2011, sysstatus 0x1, intrfsel 0x1, simenable  0x0

musb_hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine (X), bulk split (X), HB-ISO Rx (X), HB-ISO Tx (X), SoftConn)

musb_hdrc: MHDRC RTL version 1.400

musb_hdrc: setup fifo_mode 4

musb_hdrc: 29/31 max ep, 16384/16384 memory

musb_hdrc: hw_ep 0shared, max 64

musb_hdrc: hw_ep 1tx, max 512

musb_hdrc: hw_ep 1rx, max 512

musb_hdrc: hw_ep 2tx, max 512

musb_hdrc: hw_ep 2rx, max 512

musb_hdrc: hw_ep 3tx, max 512

musb_hdrc: hw_ep 3rx, max 512

musb_hdrc: hw_ep 4tx, max 512

musb_hdrc: hw_ep 4rx, max 512

musb_hdrc: hw_ep 5tx, max 512

musb_hdrc: hw_ep 5rx, max 512

musb_hdrc: hw_ep 6tx, max 512

musb_hdrc: hw_ep 6rx, max 512

musb_hdrc: hw_ep 7tx, max 512

musb_hdrc: hw_ep 7rx, max 512

musb_hdrc: hw_ep 8tx, max 512

musb_hdrc: hw_ep 8rx, max 64

musb_hdrc: hw_ep 9tx, max 512

musb_hdrc: hw_ep 9rx, max 64

musb_hdrc: hw_ep 10tx, max 512

musb_hdrc: hw_ep 10rx, max 64

musb_hdrc: hw_ep 11tx, max 256

musb_hdrc: hw_ep 11rx, max 256

musb_hdrc: hw_ep 12tx, max 256

musb_hdrc: hw_ep 12rx, max 256

musb_hdrc: hw_ep 13tx, max 256

musb_hdrc: hw_ep 13rx, max 4096

musb_hdrc: hw_ep 14shared, max 1024

musb_hdrc: hw_ep 15shared, max 1024

musb_hdrc: USB Host mode controller at d80ab000 using DMA, IRQ 92

musb_hdrc musb_hdrc: MUSB HDRC host driver

musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1

usb usb1: New USB device found, idVendor=1d6b, idProduct=0002

usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1

usb usb1: Product: MUSB HDRC host driver

usb usb1: Manufacturer: Linux 2.6.29-rc3-omap1 musb-hcd

usb usb1: SerialNumber: musb_hdrc

usb usb1: configuration #1 chosen from 1 choice

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

Registered /proc/driver/musb_hdrc

NET: Registered protocol family 2

Switched to high resolution mode on CPU 0

IP route cache hash table entries: 2048 (order: 1, 8192 bytes)

TCP established hash table entries: 8192 (order: 4, 65536 bytes)

TCP bind hash table entries: 8192 (order: 3, 32768 bytes)

TCP: Hash tables configured (established 8192 bind 8192)

TCP reno registered

NET: Registered protocol family 1

OMAP35x Linux PSP version 02.01.03.11 (OMAP3EVM)

NetWinder Floating Point Emulator V0.97 (double precision)

VFS: Disk quotas dquot_6.5.2

Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

msgmni has been set to 441

alg: No test for stdrng (krng)

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler deadline registered

io scheduler cfq registered

Generic Backlight Driver Initialized.

Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled

serial8250.0: ttyS0 at MMIO 0x4806a000 (irq = 72) is a ST16654

console [ttyS0] enabled

serial8250.0: ttyS1 at MMIO 0x4806c000 (irq = 73) is a ST16654

serial8250.0: ttyS2 at MMIO 0x49020000 (irq = 74) is a ST16654

brd: module loaded

loop: module loaded

smsc911x: Driver version 2008-10-21.

smsc911x-mdio: probed

eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=ffffffff:01, irq=-1)

net eth0: MAC Address: 00:50:c2:7e:98:67

Linux video capture interface: v2.00

usbcore: registered new interface driver uvcvideo

USB Video Class driver (v0.1.0)

i2c /dev entries driver

Driver 'sd' needs updating - please use bus_type methods

omap2-nand driver initializing

NAND device: Manufacturer ID: 0x2c, Chip ID: 0xba (Micron NAND 256MiB 1,8V 16-bit)

Creating 5 MTD partitions on "omap2-nand.0":

0x000000000000-0x000000080000 : "xloader-nand"

0x000000080000-0x000000240000 : "uboot-nand"

0x000000240000-0x000000280000 : "params-nand"

0x000000280000-0x000000780000 : "linux-nand"

0x000000780000-0x000010000000 : "jffs2-nand"

OneNAND driver initializing

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

ehci-omap ehci-omap.0: OMAP-EHCI Host Controller

ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 2

ehci-omap ehci-omap.0: irq 77, io mem 0x48064800

ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00

usb usb2: New USB device found, idVendor=1d6b, idProduct=0002

usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1

usb usb2: Product: OMAP-EHCI Host Controller

usb usb2: Manufacturer: Linux 2.6.29-rc3-omap1 ehci_hcd

usb usb2: SerialNumber: ehci-omap.0

usb usb2: configuration #1 chosen from 1 choice

hub 2-0:1.0: USB hub found

hub 2-0:1.0: 3 ports detected

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

input: omap_twl4030keypad as /class/input/input0

ads7846 spi1.0: touchscreen, irq 335

input: ADS784x Touchscreen as /class/input/input1

OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec

cpuidle: using governor ladder

cpuidle: using governor menu

usbcore: registered new interface driver usbhid

usbhid: v2.6:USB HID core driver

Advanced Linux Sound Architecture Driver Version 1.0.19.

usbcore: registered new interface driver snd-usb-audio

No device for DAI twl4030

No device for DAI twl4030 Voice

No device for DAI omap-mcbsp-dai-0

No device for DAI omap-mcbsp-dai-1

No device for DAI omap-mcbsp-dai-2

No device for DAI omap-mcbsp-dai-3

No device for DAI omap-mcbsp-dai-4

OMAP3 EVM SoC init

TWL4030 Audio Codec init

asoc: twl4030 <-> omap-mcbsp-dai-0 mapping ok

ALSA device list:

  #0: omap3evm (twl4030)

TCP cubic registered

NET: Registered protocol family 17

NET: Registered protocol family 15

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

Power Management for TI OMAP3.

SmartReflex driver initialized

Disabling unused clock "sr2_fck"

Disabling unused clock "sr1_fck"

Disabling unused clock "mcbsp_fck"

Disabling unused clock "mcbsp_fck"

Disabling unused clock "mcbsp_fck"

Disabling unused clock "mcbsp_ick"

Disabling unused clock "mcbsp_ick"

Disabling unused clock "mcbsp_ick"

Disabling unused clock "gpt2_ick"

Disabling unused clock "gpt3_ick"

Disabling unused clock "gpt4_ick"

Disabling unused clock "gpt5_ick"

Disabling unused clock "gpt6_ick"

Disabling unused clock "gpt7_ick"

Disabling unused clock "gpt8_ick"

Disabling unused clock "gpt9_ick"

Disabling unused clock "wdt3_ick"

Disabling unused clock "wdt3_fck"

Disabling unused clock "gpio2_dbck"

Disabling unused clock "gpio3_dbck"

Disabling unused clock "gpio4_dbck"

Disabling unused clock "gpio5_dbck"

Disabling unused clock "gpt9_fck"

Disabling unused clock "gpt8_fck"

Disabling unused clock "gpt7_fck"

Disabling unused clock "gpt6_fck"

Disabling unused clock "gpt5_fck"

Disabling unused clock "gpt4_fck"

Disabling unused clock "gpt3_fck"

Disabling unused clock "gpt2_fck"

Disabling unused clock "gpt12_ick"

Disabling unused clock "wdt1_ick"

Disabling unused clock "wdt2_ick"

Disabling unused clock "wdt2_fck"

Disabling unused clock "gpio1_dbck"

Disabling unused clock "des1_ick"

Disabling unused clock "sha11_ick"

Disabling unused clock "rng_ick"

Disabling unused clock "aes1_ick"

Disabling unused clock "ssi_ick"

Disabling unused clock "mailboxes_ick"

Disabling unused clock "mcbsp_ick"

Disabling unused clock "mcbsp_ick"

Disabling unused clock "gpt10_ick"

Disabling unused clock "gpt11_ick"

Disabling unused clock "hdq_ick"

Disabling unused clock "mspro_ick"

Disabling unused clock "des2_ick"

Disabling unused clock "sha12_ick"

Disabling unused clock "aes2_ick"

Disabling unused clock "icr_ick"

Disabling unused clock "pka_ick"

Disabling unused clock "ssi_ssr_fck"

Disabling unused clock "hdq_fck"

Disabling unused clock "mcbsp_fck"

Disabling unused clock "mcbsp_fck"

Disabling unused clock "mspro_fck"

Disabling unused clock "gpt11_fck"

Disabling unused clock "sad2d_ick"

Disabling unused clock "dpll4_m6x2_ck"

Disabling unused clock "dpll3_m3x2_ck"

Disabling unused clock "sys_clkout1"

VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 1

GPIO-153 autorequested

omap-dss DISPC error: Requested pixel clock not possible with the current OMAP2_DSS_MIN_FCK_PER_PCK setting. Turning the constraint off.

omap-dss: Could not find exact pixel clock. Requested 25190 kHz, got 25189 kHz

Display already enabled

Display already enabled

Buffer Size = 3686400

omap_vout: registered and initialized                   video device 0 [v4l2]

Buffer Size = 3686400

omap_vout: registered and initialized                   video device 1 [v4l2]

display->updated

net eth0: SMSC911x/921x identified at 0xd085c000, IRQ: 336

Sending DHCP requests .., OK

IP-Config: Got DHCP answer from 192.168.1.100, my address is 192.168.1.10

IP-Config: Complete:

     device=eth0, addr=192.168.1.10, mask=255.255.255.0, gw=192.168.1.1,

     host=192.168.1.10, domain=, nis-domain=(none),

     bootserver=192.168.1.100, rootserver=192.168.1.100, rootpath=/home/won/workdir/filesys

Looking up port of RPC 100003/2 on 192.168.1.100

Looking up port of RPC 100005/1 on 192.168.1.100

VFS: Mounted root (nfs filesystem) on device 0:12.

Freeing init memory: 156K

udev: starting version 141

udev: deprecated sysfs layout; update the kernel or disable CONFIG_SYSFS_DEPRECATED; some udev features will not work correctly

omap-dss: Could not find exact pixel clock. Requested 25189 kHz, got 25188 kHz

omap-dss: Could not find exact pixel clock. Requested 25188 kHz, got 25187 kHz

root@omap3evm:~#