Hi, I've seen several cases of our custom DM365 based DVR design freeze up, and when JTAG connecting to diagnose the issue, the state of PC and registers seems to point at an ARM exception, however in the wrong vector address space. The ARM TRM mentions the VINITHI signal could set the vector address to 0xffff0000, but the TMS320DM36x ARM Subsystem guide mentions that it should be always in the 0x00000000 low range. I see that UBL startup code sets up CP15 correctly to the low vector address space. Our applications are not intentionally changing anything in the supervisor processor CP15 registers, is it possible that this is some spurious error on the DM365 CPU core? I don't seem mention of this in the errata.
CPU Registers
PC 0xFFFF0010 Core Register
SP 0xC0433A2C Core Register
LR 0xFFFF0330 Core Register
CPSR 0x20000097 Core Register
R0 0xC0433A2C Core Register
R1 0xFBAD0000 Core Register
R2 0x4096A000 Core Register
R3 0x00000000 Core Register
R4 0x00000000 Core Register
R5 0x00283B34 Core Register
R6 0x00283A88 Core Register
R7 0x00000001 Core Register
R8 0x409546C4 Core Register
R9 0x00000000 Core Register
R10 0x4096A000 Core Register
R11 0xBEFE3934 Core Register
R12 0x00283B28 Core Register
ffff0010: FFFFFFFF .word 0xFFFFFFFF
ffff0014: EA00009A B 0xFFFF0284
ffff0018: EA0000FA B 0xFFFF0408
ffff001c: EA000078 B 0xFFFF0204
ffff0020: EA0000F7 B 0xFFFF0404
ffff0024: 00000000 ANDEQ R0, R0, R0
And another case
PC 0xFFFF000C Core Register
SP 0xC0433A2C Core Register
LR 0xFE7B0058 Core Register
CPSR 0xA0000097 Core Register
N 1
Z 0
C 1
V 0
Q 0
A 0
I 1
F 0
T 0
Mode 10111
R0 0x00000000 Core Register
R1 0x00000001 Core Register
R2 0x002F17A8 Core Register
R3 0x00000000 Core Register
R4 0x00000000 Core Register
R5 0x4096A000 Core Register
R6 0x002F17A8 Core Register
R7 0x002F1708 Core Register
R8 0x40022ED0 Core Register
R9 0x00000FF0 Core Register
R10 0x00000001 Core Register
R11 0x40023370 Core Register
R12 0x409546C4 Core Register
And another case:
PC 0xFFFF000C Core Register
SP 0xC0433A2C Core Register
LR 0xFE7B0058 Core Register
CPSR 0x00000097 Core Register
N 0
Z 0
C 0
V 0
Q 0
A 0
I 1
F 0
T 0
Mode 10111
R0 0x00000000 Core Register
R1 0x0025E8D8 Core Register
R2 0xE18F600C Core Register
R3 0x00000000 Core Register
R4 0xBEDF93F0 Core Register
R5 0x8F57D7FF Core Register
R6 0x401625A4 Core Register
R7 0x33713001 Core Register
R8 0xE1A03F00 Core Register
R9 0x00000000 Core Register
R10 0x40025000 Core Register
R11 0xBEDF936C Core Register
R12 0x00000000 Core Register
ffff000c: EA9F0010 B 0xFE7B0054
ffff0010: EA0000BB B 0xFFFF0304
ffff0014: EA00009A B 0xFFFF0284
ffff0018: EA0000FA B 0xFFFF0408
ffff001c: EA000078 B 0xFFFF0204
ffff000c: EA9F0010 B 0xFE7B0054
ffff0010: EA0000BB B 0xFFFF0304
ffff0014: EA00009A B 0xFFFF0284
ffff0018: EA0000FA B 0xFFFF0408
ffff001c: EA000078 B 0xFFFF0204