This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C5515, spO2 front end module, CCS 3.3 compiled but not running properly



Hi,

I am working with the EVM5515 and SpO2 front end module. I've gotten the EVM to connect to CCS3.3 by using the EVM5505 setup and replacing the gel file with the 5515. Then I built the SpO2 project and ran it, but nothing happened except the LCD lit up a bar across it. No messages or anything. I was wondering what setup is used to test the SpO2 boards, and how I can replicate that? Has anyone else on these forums gotten it to work?
Second, when I run the PC application for the SpO2 by itself, it is not able to recognize any com ports. The drop down menu is empty. Which cable is supposed to be used between the EVM and the PC? Only the microusb to usb cable works and is recognized by my PC and drivers installed. Must it be connected with serial connection?
Id appreciate any help.
Thanks very much,
Will