This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Kernel panic - not syncing: Attempted to kill init! DM355EVM

Hello everyone. I have some issues booting 2.6.32.rc2 davinci kernel on my DM355EVM

Here is the output of booting process:

DM355 EVM > tftp uImage
dm9000 i/o: 0x4014000, id: 0x90000a46
DM9000: running in 16 bit mode
MAC: 00:0e:99:02:cd:4a
operating at 100M full duplex mode
TFTP from server 10.0.2.15; our IP address is 10.0.2.17
Filename 'uImage'.
Load address: 0x80700000
Loading: #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         ###########################################################
done
Bytes transferred = 2963240 (2d3728 hex)
DM355 EVM > bootm
## Booting kernel from Legacy Image at 80700000 ...
   Image Name:   Linux-2.6.32-rc2-davinci1
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2963176 Bytes =  2.8 MB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux............................................................................................................................................................................................... done, booting the kernel.
[    0.000000] Initializing cgroup subsys cpuset
[    0.000000] Linux version 2.6.32-rc2-davinci1 (root@chapel) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #15 Sat Apr 28 15:56:04 MSK 2012
[    0.000000] CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
[    0.000000] CPU: VIVT data cache, VIVT instruction cache
[    0.000000] Machine: DaVinci DM355 EVM
[    0.000000] Memory policy: ECC disabled, Data cache writeback
[    0.000000] DaVinci dm355 variant 0x0
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 24384
[    0.000000] Kernel command line: mem=96M console=ttyS0,115200n8 root=/dev/nfs rw nfsroot=10.0.2.15:/home/spl/filesys ip=dhcp
[    0.000000] PID hash table entries: 512 (order: -1, 2048 bytes)
[    0.000000] Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
[    0.000000] Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
[    0.000000] allocated 491520 bytes of page_cgroup
[    0.000000] please try 'cgroup_disable=memory' option if you don't want memory cgroups
[    0.000000] Memory: 96MB = 96MB total
[    0.000000] Memory: 90232KB available (5600K code, 863K data, 160K init, 0K highmem)
[    0.000000] SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[    0.000000] Hierarchical RCU implementation.
[    0.000000] NR_IRQS:245
[    0.000000] Console: colour dummy device 80x30
[    0.000000] Calibrating delay loop... 107.31 BogoMIPS (lpj=536576)
[    0.230000] Security Framework initialized
[    0.230000] SELinux:  Disabled at boot.
[    0.230000] Mount-cache hash table entries: 512
[    0.230000] Initializing cgroup subsys ns
[    0.230000] Initializing cgroup subsys cpuacct
[    0.230000] Initializing cgroup subsys memory
[    0.230000] Initializing cgroup subsys devices
[    0.230000] Initializing cgroup subsys freezer
[    0.230000] CPU: Testing write buffer coherency: ok
[    0.240000] DaVinci: 104 gpio irqs
[    0.240000] regulator: core version 0.5
[    0.240000] NET: Registered protocol family 16
[    0.310000] bio: create slab <bio-0> at 0
[    0.310000] DM355 IPIPE intialized in Single Shot mode
[    0.320000] SCSI subsystem initialized
[    0.320000] vpss vpss: dm355_vpss vpss probed
[    0.320000] vpss vpss: dm355_vpss vpss probe success
[    0.320000] ch0 default output "COMPOSITE", mode "NTSC"
[    0.320000] ch1 default output "", mode ""
[    0.320000] VPBE Encoder Initialized
[    0.320000] NetLabel: Initializing
[    0.320000] NetLabel:  domain hash size = 128
[    0.320000] NetLabel:  protocols = UNLABELED CIPSOv4
[    0.330000] NetLabel:  unlabeled traffic allowed by default
[    0.330000] LogicPD encoder initialized
[    0.330000] Avnetlcd encoder initialized
[    0.330000] Switching to clocksource timer0_1
[    0.360000] musb_hdrc: version 6.0, cppi-dma, peripheral, debug=0
[    0.380000] musb_hdrc: USB Peripheral mode controller at fec64000 using DMA, IRQ 12
[    0.380000] NET: Registered protocol family 2
[    0.380000] IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
[    0.390000] TCP established hash table entries: 4096 (order: 3, 32768 bytes)
[    0.390000] TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
[    0.390000] TCP: Hash tables configured (established 4096 bind 4096)
[    0.390000] TCP reno registered
[    0.390000] NET: Registered protocol family 1
[    0.390000] RPC: Registered udp transport module.
[    0.390000] RPC: Registered tcp transport module.
[    0.390000] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.390000] audit: initializing netlink socket (disabled)
[    0.390000] type=2000 audit(0.390:1): initialized
[    0.550000] VFS: Disk quotas dquot_6.5.2
[    0.550000] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[    0.590000] NTFS driver 2.1.29 [Flags: R/W].
[    0.590000] JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
[    0.600000] ROMFS MTD (C) 2007 Red Hat, Inc.
[    0.600000] fuse init (API version 7.13)
[    0.600000] msgmni has been set to 176
[    0.610000] alg: No test for stdrng (krng)
[    0.620000] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 253)
[    0.620000] io scheduler noop registered
[    0.620000] io scheduler anticipatory registered
[    0.620000] io scheduler deadline registered
[    0.620000] io scheduler cfq registered (default)
[    0.670000] imp serializer initialized
[    0.670000] davinci_previewer initialized
[    0.670000] davinci_resizer initialized
[    0.670000] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[    0.670000] serial8250.0: ttyS0 at MMIO 0x1c20000 (irq = 40) is a 16550A
[    1.080000] console [ttyS0] enabled
[    1.090000] serial8250.0: ttyS1 at MMIO 0x1c20400 (irq = 41) is a 16550A
[    1.100000] serial8250.0: ttyS2 at MMIO 0x1e06000 (irq = 14) is a 16550A
[    1.110000] nbd: registered device at major 43
[    1.150000] SCSI Media Changer driver v0.25
[    1.160000] slram: not enough parameters.
[    1.180000] NAND device: Manufacturer ID: 0x2c, Chip ID: 0xd3 (Micron NAND 1GiB 3,3V 8-bit)
[    1.190000] 2 NAND chips detected
[    1.200000] Creating 5 MTD partitions on "davinci_nand.0":
[    1.210000] 0x000000000000-0x000000f00000 : "bootloader"
[    1.210000] 0x000000f00000-0x000001000000 : "params"
[    1.220000] 0x000001000000-0x000001400000 : "kernel"
[    1.220000] 0x000001400000-0x000021400000 : "filesystem1"
[    1.230000] 0x000021400000-0x000080000000 : "filesystem2"
[    1.250000] davinci_nand davinci_nand.0: controller rev. 2.3
[    1.270000] Fixed MDIO Bus: probed
[    1.270000] PPP generic driver version 2.4.2
[    1.280000] SLIP: version 0.8.4-NET3.019-NEWTTY (dynamic channels, max=256) (6 bit encapsulation enabled).
[    1.290000] CSLIP: code copyright 1989 Regents of the University of California.
[    1.290000] SLIP linefill/keepalive option.
[    1.300000] tun: Universal TUN/TAP device driver, 1.6
[    1.300000] tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
[    1.310000] dm9000 Ethernet Driver, V1.31
[    1.440000] eth0: dm9000a at c6ca6000,c6caa002 IRQ 65 MAC: 00:0e:99:02:cd:4a (eeprom)
[    1.450000] console [netcon0] enabled
[    1.450000] netconsole: network logging started
[    1.460000] g_file_storage gadget: no file given for LUN0
[    1.470000] mice: PS/2 mouse device common for all mice
[    1.470000] i2c /dev entries driver
[    1.480000] Linux video capture interface: v2.00
[    1.480000] af major#: 250, minor# 0
[    1.490000] aew major#: 249, minor# 0
[    1.490000] watchdog watchdog: heartbeat 60 sec
[    1.500000] cpuidle: using governor ladder
[    1.500000] cpuidle: using governor menu
[    1.520000] TCP cubic registered
[    1.520000] Initializing XFRM netlink socket
[    1.530000] NET: Registered protocol family 17
[    1.530000] NET: Registered protocol family 33
[    1.540000] registered taskstats version 1
[    1.550000] drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
[    2.100000] eth0: link down
[    2.460000] eth0: link up, 100Mbps, full-duplex, lpa 0xCDE1
[    3.110000] Sending DHCP requests ., OK
[    3.340000] IP-Config: Got DHCP answer from 10.0.2.15, my address is 10.0.2.17
[    3.340000] IP-Config: Complete:
[    3.350000]      device=eth0, addr=10.0.2.17, mask=255.0.0.0, gw=255.255.255.255,
[    3.350000]      host=10.0.2.17, domain=example.org, nis-domain=(none),
[    3.360000]      bootserver=10.0.2.15, rootserver=10.0.2.15, rootpath=
[    3.370000] Looking up port of RPC 100003/2 on 10.0.2.15
[    3.390000] Looking up port of RPC 100005/1 on 10.0.2.15
[    3.410000] VFS: Mounted root (nfs filesystem) on device 0:14.
[    3.420000] Freeing init memory: 160K
[    3.520000] Kernel panic - not syncing: Attempted to kill init!
[    3.520000] Backtrace:
[    3.530000] [<c00346c0>] (dump_backtrace+0x0/0x114) from [<c0458b78>] (dump_stack+0x20/0x24)
[    3.540000]  r6:c05e12dc r5:c05b26b0 r4:c05b26b0
[    3.540000] [<c0458b58>] (dump_stack+0x0/0x24) from [<c0458bd0>] (panic+0x54/0x134)
[    3.550000] [<c0458b7c>] (panic+0x0/0x134) from [<c004f634>] (do_exit+0x6cc/0x700)
[    3.560000]  r3:60000013 r2:c4023e38 r1:c4023c0c r0:c0522cf4
[    3.560000] [<c004ef68>] (do_exit+0x0/0x700) from [<c004f6b4>] (do_group_exit+0x4c/0xcc)
[    3.570000] [<c004f668>] (do_group_exit+0x0/0xcc) from [<c005e888>] (get_signal_to_deliver+0x1c8/0x380)
[    3.580000]  r4:c4022000
[    3.580000] [<c005e6c0>] (get_signal_to_deliver+0x0/0x380) from [<c0032f24>] (do_notify_resume+0xc8/0x5c0)
[    3.590000] [<c0032e5c>] (do_notify_resume+0x0/0x5c0) from [<c0030a68>] (work_pending+0x1c/0x20)

So everything goes fine before userspace attachment. Any suggestions?

Im using filesystem from dvsdk 3.10 "arago-demo-image-dm355-evm.tar.gz" , is it right?

Best regards. Pavel Goryunov.