I just updated to version 2.6.0 from Appro's FTP site. I did not build from source, and used the uImage and cramfs from the Application/bin/Dm368 directory. When using the Web application in the camera, the Add/Edit Users and Settings | Network and Port features produce an error from the Web application "GBasic Error | Form Object Property Not Found".
I have also seen people in other conversations discuss version 2.6.2. I tried the cramfs from the Patch directory, and the version still reads 2.6.0. How do I get to version 2.6.2, and does t fix the GBasic error issue? I have also seen that a version 3.0 exists, but I have not seen any information on obtaining this version, and looking on Appro's FTP site only shows version 2.6. How do I get version 3.0?