Dear all,
I had checked DM365EVM layout file on DDR2 trace as below.
1. DDR_GATE0 to DDR_GATE1: 2511.97(383.08+2128.89)
2. CLKP: 1590.79(738.12+852.67)
3. DQ0~15: 1374.148(average)
The DM365EVM schematic had mentioned that the DDR_GATE net is equal to the DDR_CLKP ( or DDR_CLKN ) plus the length of DDR_DQXX average trace length. But the length is 2511.97 not 2964 in the EVM layout. Can anyone help me to explain this portion? Thanks in advance.
B.R.
OC