Hi,
I know DM8168 VIP port support embedded sync 16bit YUV422, but know, I want to know which format does support, such as BT.1120? SMPTE 274M or SMPTE 292M or others?
thanks!
puyol.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I know DM8168 VIP port support embedded sync 16bit YUV422, but know, I want to know which format does support, such as BT.1120? SMPTE 274M or SMPTE 292M or others?
thanks!
puyol.
All parallel formats are supported directly and in fact any resolution and pixel rate up to 1920x1200 and 165MHz is supported.
SMPTE 292M is a serial format and is not directly supported, but could be supported with an external de-serializer.
BR,
Steve
Hi,
Just once more addition.
1920X1200 is supported with reduced blanking. Standard VESA timings for 1920X1200 requires 193MHz clock.
Regards,
Hardik Shah