This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Setting-Up BeagleBone for TFTP App Downloading



I want to setup my beaglebone board to tftp my application from my windows host machine using a static IP and not DHCP which appears to be the default configuration. The beaglebone does not appear to have a boot.cmd file to modify and I'm not sure what ethernet parameters to use for this board.

Looking for some assistance on where and how to configure the beaglebone board with a statis IP of 10.0.0.3 and what changes are needed to tftp from host IP of 10.0.0.1

Thanks