Hi,
I am using a a custom board which is similar to blaze but uses omap 4460 processor.I am using ICS on my custom board.There was no HAL for gyroscope so i wrote my own HAL but i am not getting any values for X Y and Z.Below is the code i wrote.The driver works fine.
Following is my HAL code:
#include <fcntl.h>
#include <errno.h>
#include <math.h>
#include <poll.h>
#include <unistd.h>
#include <dirent.h>
#include <sys/select.h>
#include <cutils/log.h>
#include "ewtsa.h"
#define FETCH_FULL_EVENT_BEFORE_RETURN 0
/*****************************************************************************/
ewtsaSensor::ewtsaSensor()
: SensorBase(NULL, "ewtsa"),
mEnabled(0),
mInputReader(4),
mHasPendingEvent(false)
{
mPendingEvent.version = sizeof(sensors_event_t);
mPendingEvent.sensor = ID_GY;
mPendingEvent.type = SENSOR_TYPE_GYROSCOPE;
memset(mPendingEvent.data, 0, sizeof(mPendingEvent.data));
if (data_fd) {
strcpy(input_sysfs_path, "/sys/bus/i2c/drivers/ewtsa/4-0068/");
input_sysfs_path_len = strlen(input_sysfs_path);
}
}
ewtsaSensor::~ewtsaSensor() {
if (mEnabled) {
enable(0, 0);
}
}
int ewtsaSensor::setInitialState() {
struct input_absinfo absinfo_x;
struct input_absinfo absinfo_y;
struct input_absinfo absinfo_z;
float value;
if (!ioctl(data_fd, EVIOCGABS(EVENT_TYPE_GYRO_X), &absinfo_x) &&
!ioctl(data_fd, EVIOCGABS(EVENT_TYPE_GYRO_X), &absinfo_y) &&
!ioctl(data_fd, EVIOCGABS(EVENT_TYPE_GYRO_X), &absinfo_z)) {
value = absinfo_x.value;
mPendingEvent.data[0] = value * CONVERT_GYRO_X;
value = absinfo_x.value;
mPendingEvent.data[1] = value * CONVERT_GYRO_Y;
value = absinfo_x.value;
mPendingEvent.data[2] = value * CONVERT_GYRO_Z;
mHasPendingEvent = true;
}
return 0;
}
int ewtsaSensor::enable(int32_t, int en) {
int flags = en ? 1 : 0;
if (flags != mEnabled) {
int fd;
strcpy(&input_sysfs_path[input_sysfs_path_len],"enable");
fd = open(input_sysfs_path, O_RDWR);
if (fd >= 0) {
char buf[2];
int err;
buf[1] = 0;
if (flags) {
buf[0] = '1';
} else {
buf[0] = '0';
}
err = write(fd, buf, sizeof(buf));
close(fd);
mEnabled = flags;
setInitialState();
return 0;
}
return -1;
}
return 0;
}
63,1 43%
bool ewtsaSensor::hasPendingEvents() const {
return mHasPendingEvent;
}
int ewtsaSensor::setDelay(int32_t handle, int64_t delay_ns)
{
int fd;
strcpy(&input_sysfs_path[input_sysfs_path_len], "delay");
fd = open(input_sysfs_path, O_RDWR);
if (fd >= 0) {
char buf[80];
int32_t delay_ms = (int32_t)delay_ns/1000000;
sprintf(buf, "%d", delay_ms);
write(fd, buf, strlen(buf)+1);
close(fd);
return 0;
}
return -1;
}
int ewtsaSensor::readEvents(sensors_event_t* data, int count)
{
if (count < 1)
return -EINVAL;
if (mHasPendingEvent) {
mHasPendingEvent = false;
mPendingEvent.timestamp = getTimestamp();
*data = mPendingEvent;
return mEnabled ? 1 : 0;
}
ssize_t n = mInputReader.fill(data_fd);
if (n < 0)
return n;
int numEventReceived = 0;
input_event const* event;
#if FETCH_FULL_EVENT_BEFORE_RETURN
again:
#endif
while (count && mInputReader.readEvent(&event)) {
int type = event->type;
if (type == EV_REL) {
float value = event->value;
if (event->code == EVENT_TYPE_GYRO_X) {
mPendingEvent.data[0] = value * CONVERT_GYRO_X;
} else if (event->code == EVENT_TYPE_GYRO_Y) {
mPendingEvent.data[1] = value * CONVERT_GYRO_Y;
} else if (event->code == EVENT_TYPE_GYRO_Z) {
mPendingEvent.data[2] = value * CONVERT_GYRO_Z;
}
} else if (type == EV_SYN) {
mPendingEvent.timestamp = timevalToNano(event->time);
if (mEnabled) {
*data++ = mPendingEvent;
count--;
numEventReceived++;
}
} else {
LOGE("ewtsa: unknown event (type=%d, code=%d)",
type, event->code);
}
mInputReader.next();
}
#if FETCH_FULL_EVENT_BEFORE_RETURN
167,1 91%
try again instead of returning with nothing and redoing poll. */
if (numEventReceived == 0 && mEnabled == 1) {
n = mInputReader.fill(data_fd);
if (n)
goto again;
}
#endif
return numEventReceived;
}
179,0-1 Bot
Please tell me what change I have to do here
Thanks
Haran