This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

problem in getting displaying output from c6713n CRO



hello all,

i am doing a sppech processing project using TMS320c6713 dsk.,before staring the actul project i tried to run the code given below( from rulpha chassing book)I attatched all the following files c6713dskinit.c,c6713dskinit.h,rts6700lib,dsk6713bsl.libcsl6713.lib,vectors_intr.asm and hello.cmd(using ccs version 3.0).the project was copmiled and built without any errors..I connected signal generator to linein and oscilloscope to line out,but didnot get anything on CRO neither on output window of ccs(RUNNING was being dislayed).Please tell me what is the problem.

#include "bs2700.cof" //coefficient file

#include "dsk6713_aic23.h" //codec-dsk support file

Uint32 fs=DSK6713_AIC23_FREQ_8KHZ; //set sampling rate

int yn = 0; //initialize filter's output

short dly[N]; //delay samples

interrupt void c_int11() //ISR

{

short i;

dly[0]=input_sample(); //input newest sample

yn = 0; //initialize filter's output

for (i = 0; i< N; i++)

yn += (h[i] * dly[i]); //y(n) += h(i)* x(n-i)

for (i = N-1; i > 0; i--) //starting @ end of buffer

dly[i] = dly[i-1]; //update delays with data move

output_sample(yn >> 15); //scale output filter sample

return;

}

void main()

{

comm_intr(); //init DSK, codec, McBSP

while(1); //infinite loop

}

thank you.

 

  • What is CRO?

    Put a breakpoint in the ISR and see if you ever get there.

    Take a look at the assembly for the while(1) loop. If it is too tight, you might never get interrupts. But if you compiled with Debug Configuration (recommended for now for debugging) then it is probably not too tight. Too tight means it is a 6-cycle or smaller loop that might not be interruptible.

    Regards,
    RandyP