Hi,
I've been working with the OMAPL-138 LogicPD SOM and have developed code for both the ARM and DSP. I would now like to create an SPI bootable version of code which is a combination of both the ARM and DSP code I've mentioned.
I've looked on the Starter Ware Wiki for a procedure or process that explains how to do this but at this point am still confused.
There are at least three support / utility applications mentioned: out2rprc, AISGen and the serial FLASH Writer.
If anyone knows the sequence of how these utilities should be used to create and install an ARM+DSP SPI FALSH Boot code can you please outline the process?
Also does anyone know if the code can be flased into the SPI FLASH using CCS and the Spectrum Digtial JTAG
Thanks!