Other Parts Discussed in Thread: PMP
Hi,
I am using the SATA0 Port from DM814X to connect the external Hard disk. Instead of 3Gbps the Target and host is able to communicate only with 1.5Gbps. Sometime Target identifies the link to be 3.0Gbps but during communication the speed is limited to 1.5Gbps. Following are the error messages.
ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 300)
ata1: hard resetting link
ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 300)
ata1: hard resetting link
ata1: SATA link down (SStatus 0 SControl 300)
ata1: hard resetting link
ata1: SATA link down (SStatus 0 SControl 300)
ata1: limiting SATA link speed to 1.5 Gbps
ata1: hard resetting link
ata1: SATA link down (SStatus 0 SControl 310)
ata1: limiting SATA link speed to 1.5 Gbps
Layout Details:
1. Max total length of trace from SOC to HDD is 3.7inch (Pairs length matched within 5mil)
2. SATA passes in 2 modules separated by a B2B connector BSH/BTH Series Samtec Connector.
3. Molex/Foxconn SATA Cable is used to interface Hard Disk.
What can be reason for this?
Regards,
Kinjan