This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8127 u-boot problem



I just received version_2.8.0 from appropho for DM8127 and tried to upgrade the u-boot. I followed the same commands as given in the user guide and in /binaries/update.txt. 

To burn u-boot.min.nand

tftp 0x81000000 u-boot.min.nand

nand erase 0x0 0x20000

nand write.i 0x81000000 0x0 0x20000

To burn u-boot.bin

tftp 0x81000000 u-boot.bin

nand erase 0x20000 0x60000

nand write.i 0x81000000 0x20000 0x60000

The burning took place successfuly (I got messages). But when I power reset the camera, it just shows a repeated "CCCCCCC................" message and doesn't move ahead. What is the problem? I will really appreciate any help in this regard.

Khan,

  • Hi Khan,

    Sorry that the memory initialization is missing in the above commands given in update.txt, even I'm not sure if this really caused the problem, please use the commands given in the user guide henceforth:

    To burn u-boot.min.nand

    mw.b 0x81000000 0xFF 0x20000

    tftp 0x81000000 u-boot.min.nand

    nand erase 0x0 0x20000

    nand write.i 0x81000000 0x0 0x20000

    To burn u-boot.bin

    mw.b 0x81000000 0xFF 0x60000

    tftp 0x81000000 u-boot.bin

    nand erase 0x20000 0x60000

    nand write.i 0x81000000 0x20000 0x60000

     

    Now, the camera shows CCC means it cannot find a valid UBL, and it's waiting for loading UBL from UART.

    If you have CCS installed you can refer to the section 1.5.1 in the user guide to flash UBL using CCS.

    Otherwise, you can also transfer UBL via minicom or teraterm. When the camera is printing CCC, from TeraTerm Menu click "File -> Transfer -> Kermit -> Send". Select the 1st stage u-boot image "u-boot.min.nand" and click "OPEN" button. The camera will receive and load this UBL automatically (but not burned to flash) and you will get the UBL prompt again. From there you can follow the section 1.5.2.

     

  • Hi!

     

    The exact same thing happened to me: trying to upgrade u-boot from 2.8.0  via tftp from u-boot --> camer print CCCC

    The only difference is I did not forget memory initialization.

    Khan, were you able to recover u-boot? 

    I was able to boot ubl over UART with minicom. I uploaded u-boot as well, but when I try to load it, it hangs.

    This is what I do, and what I get:

     

    ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
    TI-MIN#go 0x81000000
    ## Starting application at 0x81000000 ...


    U-Boot 2010.06 (May 29 2012 - 16:19:17)

    TI8148-GP rev 2.1

    ARM clk: 600MHz
    DDR clk: 400MHz
    L3 clk: 200MHz
    IVA clk: 450MHz
    ISS clk: 400MHz
    DSP clk: 500MHz
    DSS clk: 200MHz

    I2C: ready
    DRAM: 2 GiB
    NAND: HW ECC BCH8 Selected
    256 MiB
    MMC: OMAP SD/MMC: 0

    ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ 

     System hangs here.

    What could be the problem?

    Thanks in advance! 

    --

     

  • Hi 

    I followed the update.txt. I can updated U-boot but I can not mount the NFS.

    that is what happen to me.

    thanks

  • Hi,

    We are using DM8127. I uploaded u-boot as well, but when I try to load it, it hangs u-boot on DM8127. CPSW register function call hanges . no console is available. See below log for  DM8127. & check also SP is 0x0000000 using JATG

    ARM clk: 600MHz
    DDR clk: 533MHz
    L3 clk:  200MHz
    IVA clk: 450MHz
    ISS clk: 400MHz
    DSP Default OFF
    DSS Default OFF

    I2C:   ready
    DRAM:  512 MiB
    DCACHE:  On
    NAND:  HW ECC BCH8 Selected
    NAND device: Manufacturer ID: 0x2c, Chip ID: 0xdc (Micron NAND 512MiB 3,3V 8-bit)
    NAND bus width 16 instead 8 bit
    No NAND device found!!!
    0 MiB
    MMC:   OMAP SD/MMC: 0, ON-BOARD SDIO: 1
    *** Warning - bad CRC or NAND, using default environment

    Net:   <ethaddr> not set. Reading from E-fuse
    Detected MACID:84:7e:40:fa:fc:a2

  • Hi Tejas Patil,

    tejas patil said:
    We are using DM8127

    Is this DM8127 TI EVM or DM8127 custom board?

    tejas patil said:
     I uploaded u-boot as well, but when I try to load it, it hangs u-boot on DM8127.

    How you built your u-boot? How you load your u-boot (UART, MMC/SD, etc)?

    tejas patil said:
    CPSW register function call hanges

    tejas patil said:
    Detected MACID:84:7e:40:fa:fc:a2

    Have you made some modifications in the u-boot source code?

    Regards,
    Pavel

  • Hi pavel,

    1) DM8127 custom board

    2)  make CROSS_COMPILE=arm-arago-linux-gnueabi- ARCH=arm ti8148_ipnc_min_uart (Base code for U-Boot RDK IPNC_RDK_V3.8.0.tar.gz for DM8127 SoC)

    3) No modification done in u-boot .

    Regards,
    Tejas patil

  • Tejas,

    tejas patil said:
    1) DM8127 custom board

    Do you have ethernet hardware in your custom board (like we have in the TI EVM)? Do you have ethernet PHY? If yes, is it the same as in the TI EVM?

    tejas patil said:
    2)  make CROSS_COMPILE=arm-arago-linux-gnueabi- ARCH=arm ti8148_ipnc_min_uart (Base code for U-Boot RDK IPNC_RDK_V3.8.0.tar.gz for DM8127 SoC)

    Are you building just the 1st stage bootloader (u-boot.min.uart)? When I load/start just the 1st stage bootloader in DM814x TI EVM, I have:

    U-Boot 2010.06 (Nov 04 2014 - 17:04:35)

    TI8148-GP rev 2.1

    ARM clk: 600MHz
    DDR clk: 400MHz

    DRAM:  1 GiB
    DCACHE:  Off
    Using default environment

    The 2nd stage U-Boot will now be auto-loaded
    Please do not interrupt the countdown till TI8148_EVM prompt if 2nd stage is already flashed
    Hit any key to stop autoboot:  0
    TI-MIN#


    Then I build my 2nd stage bootloader (u-boot.bin) and when load/start I have:

    TI-MIN#go 0x80008000
    ## Starting application at 0x80008000 ...


    U-Boot 2010.06 (Nov 04 2014 - 17:05:28)

    TI8148-GP rev 2.1

    ARM clk: 600MHz
    DDR clk: 400MHz

    I2C:   ready
    DRAM:  1 GiB
    DCACHE:  On
    NAND:  HW ECC BCH8 Selected
    256 MiB
    MMC:   OMAP SD/MMC: 0
    *** Warning - bad CRC or NAND, using default environment

                              .:;rrr;;.                   
                        ,5#@@@@#####@@@@@@#2,             
                     ,A@@@hi;;;r5;;;;r;rrSG@@@A,          
                   r@@#i;:;s222hG;rrsrrrrrr;ri#@@r        
                 :@@hr:r;SG3ssrr2r;rrsrsrsrsrr;rh@@:      
                B@H;;rr;3Hs;rrr;sr;;rrsrsrsrsrsr;;H@B     
               @@s:rrs;5#;;rrrr;r#@H:;;rrsrsrsrsrr:s@@    
              @@;;srs&X#9;r;r;;,2@@@rrr:;;rrsrsrsrr;;@@   
             @@;;rrsrrs@MB#@@@@@###@@@@@@#rsrsrsrsrr;;@@  
            G@r;rrsrsr;#X;SX25Ss#@@#M@#9H9rrsrsrsrsrs;r@G
            @9:srsrsrs;2@;:;;:.X@@@@@H::;rrsrsrsrsrsrr:3@
           X@;rrsrsrsrr;XAi;;:&@@#@Bs:rrsrsrsrsrsrsrsrr;@X
           @#;rsrsrsrsrr;r2ir@@@###::rrsrsrsrsrsrsrsrsr:@@
           @A:rrsrsrsrr;:2@29@@M@@@;:;rrrrsrsrsrsrsrsrs;H@
           @&;rsrsrsrr;A@@@@@@###@@@s::;:;;rrsrsrsrsrsr;G@
           @#:rrsrsrsr;G@5Hr25@@@#@@@#9XG9s:rrrrsrsrsrs:#@
           M@;rsrsrsrs;r@&#;::S@@@@@@@M@@@@Grr:;rsrsrsr;@#
           :@s;rsrsrsrr:M#Msrr;;&#@@@@@@@@@@H@@5;rsrsr;s@,
            @@:rrsrsrsr;S@rrrsr;:;r3MH@@#@M5,S@@irrsrr:@@
             @A:rrsrsrsrrrrrsrsrrr;::;@##@r:;rH@h;srr:H@  
             ;@9:rrsrsrsrrrsrsrsrsr;,S@Hi@i:;s;MX;rr:h@;  
              r@B:rrrrsrsrsrsrsrr;;sA@#i,i@h;r;S5;r:H@r   
               ,@@r;rrrsrsrsrsrr;2BM3r:;r:G@:rrr;;r@@,    
                 B@Mr;rrrrsrsrsr@@S;;;rrr:5M;rr;rM@H      
                  .@@@i;;rrrrsrs2i;rrrrr;r@M:;i@@@.       
                    .A@@#5r;;;r;;;rrr;r:r#AsM@@H.         
                       ;&@@@@MhXS5i5SX9B@@@@G;            
                           :ihM#@@@@@##hs,                

    Net:   <ethaddr> not set. Reading from E-fuse
    Detected MACID:90:d7:eb:d5:13:96
    cpsw
    Hit any key to stop autoboot:  0
    TI8148_EVM#


    Please provide more details about you boot source (UART, MMC/SD, NAND, etc).

    tejas patil said:
    3) No modification done in u-boot .

    Can you try comment/disable the cpsw_eth_set_mac_addr(mac_addr) function:

    u-boot/board/ti/<ti8127 ipnc>/evm.c

    int board_eth_init(bd_t *bis)
    {

    if(is_valid_ether_addr(mac_addr)) {
            printf("Detected MACID:%x:%x:%x:%x:%x:%x\n",mac_addr[0],
                mac_addr[1], mac_addr[2], mac_addr[3],
                mac_addr[4], mac_addr[5]);
          //  cpsw_eth_set_mac_addr(mac_addr);  ---> comment here

    Thus we will be sure your code stuck in this function.

    Best regards,
    Pavel

  • Hi pavel,

    i was //  cpsw_eth_set_mac_addr(mac_addr);  ---> comment here but till it hanges it is hanges in

    return cpsw_register(&cpsw_data);

    Best regards,

    Tejas

  • Pavel Botev said:
    Do you have ethernet hardware in your custom board (like we have in the TI EVM)? Do you have ethernet PHY? If yes, is it the same as in the TI EVM?

    Pavel Botev said:
    Are you building just the 1st stage bootloader (u-boot.min.uart)?

    Pavel Botev said:
    Please provide more details about you boot source (UART, MMC/SD, NAND, etc).

  • Hi pavel

    1.Do you have ethernet hardware in your custom board (like we have in the TI EVM)? Do you have ethernet PHY? If yes, is it the same as in the TI EVM?
     
    -Yes but not same as TI EVM. ETherent PHY is different KSZ9031 PHY. RGMII  mode is used.
    2. Are you building just the 1st stage bootloader (u-boot.min.uart)?
     
    -Building both min and max bootloader
    3.Please provide more details about you boot source (UART, MMC/SD, NAND, etc).
    -Boot source is UART.
    Plz find attached evm,.c file with my changes.
  • Tejas,

    tejas patil said:

    i was //  cpsw_eth_set_mac_addr(mac_addr);  ---> comment here but till it hanges it is hanges in

    return cpsw_register(&cpsw_data);

    Can you try the above modification:

    //return cpsw_register(&cpsw_data);
    return 1;

    }

    After this change, will your u-boot hang or load up successful (even without cpsw support)?

    BR
    Pavel

  • Hi pavel,

    Boot log after return 1 load up successful but without cpsw support.

    Phy1 Reset initialized
    Net:   <ethaddr> not set. Reading from E-fuse
    Detected MACID:d0:39:72:67:4a:ec
    No ethernet found. Enter stop in 3 seconds to stop autoboot


    BR

    Tejas

  • Tejas,

    tejas patil said:
    1.Do you have ethernet hardware in your custom board (like we have in the TI EVM)? Do you have ethernet PHY? If yes, is it the same as in the TI EVM?
     
    -Yes but not same as TI EVM. ETherent PHY is different KSZ9031 PHY. RGMII  mode is used.

    The DM814x/DM811x TI EVMs has AR8031 PHYs, working in RGMII mode. So RGMII mode should no be the problem. Please see the below pointers regarding using different ethernet PHY:

    http://processors.wiki.ti.com/index.php/TI81xx_PSP_Porting_Guide#Ethernet_Driver_-_Adding_Custom_Ethernet_Phy

    http://e2e.ti.com/support/embedded/linux/f/354/t/218006.aspx

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/209865.aspx

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/349885.aspx

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/358952.aspx

    I can also suggest you to try with the latest u-boot code base:

    http://arago-project.org/git/projects/?p=u-boot-ipnc-rdk-dm81xx.git;a=shortlog;h=refs/heads/ipncrdk_psp_dm81xx_uboot

    BR
    Pavel

  • Tejas,

    tejas patil said:
    Boot log after return 1 load up successful but without cpsw support.

    Can you try explore the u-boot/drivers/net/cpsw.c cpsw_register() function:

    int cpsw_register(struct cpsw_platform_data *data)
    {
        struct cpsw_priv    *priv;
        void            *regs = (void *)data->cpsw_base;
        struct eth_device    *dev;

        dev = malloc(sizeof(*dev));
        if (!dev)
            return -ENOMEM;
        memset(dev, 0, sizeof(*dev));

        priv = malloc(sizeof(*priv));
        if (!priv) {
            free(dev);
            return -ENOMEM;
        }
        memset(priv, 0, sizeof(*priv));

        priv->data = *data;
        priv->dev  = dev;

        priv->slaves = malloc(sizeof(struct cpsw_slave) * data->slaves);
        if (!priv->slaves) {
            free(dev);
            free(priv);
            return -ENOMEM;
        }

        priv->host_port         = data->host_port_num;
        priv->regs        = regs;
        priv->host_port_regs    = regs + data->host_port_reg_ofs;
        priv->dma_regs        = regs + data->cpdma_reg_ofs;
        priv->dma_sram_regs    = regs + data->cpdma_sram_ofs;
        priv->ale_regs        = regs + data->ale_reg_ofs;
        priv->descs        = regs + data->bd_ram_ofs;

        for_each_slave(priv, cpsw_slave_setup, idx, priv);

        strcpy(dev->name, "cpsw");
        dev->iobase    = 0;
        dev->init    = cpsw_init;
        dev->halt    = cpsw_halt;
        dev->send    = cpsw_send;
        dev->recv    = cpsw_recv;
        dev->priv    = priv;

        eth_register(dev);

        cpsw_mdio_init(dev->name, data->mdio_base, data->mdio_div);

        return 1;
    }

    Can you put printf statements and see where exactly your flow stuck (in eth_register(dev), or in cpsw_mdio_init() or else).

    BR
    Pavel

  • Hi pavel,

    It is hangs in cpsw_mdio_init(dev->name, data->mdio_base, data->mdio_div); function

    below function is hangs after this commented cpsw is register .

            /* set enable and clock divider */
     __raw_writel(div | CONTROL_ENABLE, &mdio_regs->control); and dhcp & tftpboot command is not working

    Net:   <ethaddr> not set. Reading from E-fuse
    Detected MACID:d0:39:72:67:4a:ec
    cpsw
    Hit any key to stop autoboot:  0
    TI8148_IPNC#
    TI8148_IPNC#dhcp

    no print at output at dhcp command is used

    BR

    Tejas

  • Tejas,

    tejas patil said:

    It is hangs in cpsw_mdio_init(dev->name, data->mdio_base, data->mdio_div); function

    below function is hangs after this commented cpsw is register .

            /* set enable and clock divider */
     __raw_writel(div | CONTROL_ENABLE, &mdio_regs->control); and dhcp & tftpboot command is not working

    This line is trying to enable the MDIO:

    MDIO CONTROL[30] ENABLE = 1 - Enable control.  Enable the MDIO state machine.

    Can you check if you can access (read/write) the MDIO registers at all? You can put one printf like below:

    static void cpsw_mdio_init(char *name, u32 mdio_base, u32 div)
    {
        mdio_regs = (struct cpsw_mdio_regs *)mdio_base;
        
        printf("mdio_regs->control = %x\n",__raw_readl(0x4A100804));

        /* set enable and clock divider */
        __raw_writel(div | CONTROL_ENABLE, &mdio_regs->control);

    The when loading u-boot, you should have:

    Net:   <ethaddr> not set. Reading from E-fuse
    Detected MACID:90:d7:eb:d5:13:96
    mdio_regs->control = 810000ff

  • Hi pavel,

    mdio_regs->control = 810000ff
    Ethernet is working ok .thank you pavel

    BR

    tejas

  • Tejas,

    tejas patil said:
    printf("mdio_regs->control = %x\n",__raw_readl(0x4A100804)); read it is hangs in this function also.

    In order to be able to access (read/write) the MDIO registers (starting from address 0x4A100800) you should enable the clock signals:

    TRM, chapter 3PSW Ethernet Subsystem (EMAC)

    9.3.4 Initialization and Configuration of CPSW
    To configure the 3PSW Ethernet Subsystem for operation the host must perform the following:
    1. Select the Interface (G/MII, RGMII, RMII) Mode
    2. Configure pads (PIN muxing), as per the interface selected.
    3. Enable the 3PSW Ethernet Subsystem Clocks
    4. Configure the PRCM registers CM_ETHERNET_CLKSTCTRL, CM_ALWON_ETHERNET_0_CLKCTRL to enable power and clocks to 3PSW Ethernet Subsystem
    5. ....

    Let me check step 4. Could you print the PRCM registers value:

    static void cpsw_mdio_init(char *name, u32 mdio_base, u32 div)
    {
        mdio_regs = (struct cpsw_mdio_regs *)mdio_base;
       
        printf("CM_ETHERNET_CLKSTCTRL = %x\n",__raw_readl(0x48181404));
        printf("CM_ALWON_ETHERNET_0_CLKCTRL = %x\n",__raw_readl(0x481815D4));

        /* set enable and clock divider */
        __raw_writel(div | CONTROL_ENABLE, &mdio_regs->control);

    When load the new u-boot, I have:

    Net:   <ethaddr> not set. Reading from E-fuse
    Detected MACID:90:d7:eb:d5:13:96
    CM_ETHERNET_CLKSTCTRL = 302
    CM_ALWON_ETHERNET_0_CLKCTRL = 2
    cpsw

    BR
    Pavel

  • Hi pavel,

    Thank's. Ethernet is working ok

    BR

    Tejas

  • Tejas,

    tejas patil said:
    Thank's. Ethernet is working ok

    Do you mean that your u-boot no more stuck and register cpsw successful?

    BR
    Pavel

  • Hi pavel,

    Yes , register cpsw successful .

    BR

    Tejas

  • Tejas,

    Could you please share, in short, what was the root cause, was it the value in PRCM registers?

    BR
    Pavel

  • Hi pavel,

    Hi,

    I am using DM8127 custom board. I am using UART1 port loop back  ttyO1

    echo "Hello" > /dev/ttyO1;cat /dev/ttyO1 nothing on output ??

    BR

    Tejas

  • Tejas,

    tejas patil said:

    Hi,

    I am using DM8127 custom board. I am using UART1 port loop back  ttyO1

    echo "Hello" > /dev/ttyO1;cat /dev/ttyO1 nothing on output ??

    Please open new thread for questions not related to the current e2e thread.

    BR