Hi,
did anyone already succeed in running a custom linux kernel (i.e., not the one from EZSDK) on the DM816x EVM?
So far I've tried kernel 3.2 from Ubuntu 12.04 Desktop for ARM/OMAP3, and vanilla 2.6.37.6 and 3.3.4 from kernel.org.
The Ubuntu kernel at least seems to recognize the EVM, but then gives the following error:
[ 0.000000] Linux version 3.2.0-23-omap (buildd@ishigaq) (gcc version 4.6.3 (Ubuntu/Linaro 4.6.3-1ubuntu4) ) #36-Ubuntu Tue Apr 10 20:24:21 UTC 2012 (Ubuntu 3.2.0-23.36-omap 3.2.14) [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d ... [ 0.000000] Machine: ti8168evm ... [ 0.000000] TI816X ES1.1 (neon ) [ 0.000000] Unhandled fault: external abort on non-linefetch (0x1028) at 0xfa17f8e4 [ 0.000000] Internal error: : 1028 [#1]
The vanilla kernels both hang after: "Starting kernel ..."
Does anybody have an idea what's wrong here?
Thanks!