All:
DSP_BIOS 5.41.11.38, TMS320C5505
I would like to be able to access the comment field of the HWI_INTx to change it to something meaningful, like DMA Interrupt for HWI_INT8. It can be very confusing to someone who is going to be using code that I have written. Is there a way to turn on the comment fields in the HWI module, or will they remain grayed out?