Other Parts Discussed in Thread: TVP7002
I'm getting an I2C timeout with EZSDK 5.04.00.11 that is not happening with 5.03.01.15.
I'm new with TDM8168EVM and I'm trying to do something with gstreamer. I've been unable to get anything to work with 5.03 and when I saw 5.04 is supported on my host OS (U11.10), I decided to see if that works any better.
After install and setup.sh of EZSDK, both versions were built using the mksdboot.sh script. I copied /usr/share/ti/ti-media-controller-utils/load-hd-v4l2-firmware.sh to /etc/init.d/load-hd-firmware.sh. And what follows is the boot output from each. I've done some searching and reading, and two possible explanations have been presented: 1. the boards need to be reseated and 2. using the wrong version of drivers. Since I've never had the boards apart and there isn't an issue on the previous version, I doubt #1 is the problem. Since I've built from the canned distribution of EZSDK, how could the drivers be the wrong version? I create the 5.03 SD from a U10.04 VirtualBox VM while the 5.04 SD is done native in U11.10. There is no cross contamination possible. I'd like to stay with EZSDK 5.04, if at all possible.
5.03
SysLink version : 2.00.05.85
SysLink module created on Date:Dec 9 2011 Time:12:47:37
FIRMWARE: Memory map bin file not passed
Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [Location of Mem map bin file]
FIRMWARE: Default memory configuration is used
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.1.1
FIRMWARE: Memory Configuration status : In Progress
FIRMWARE: 1 start Successful
Loading HDVPSS (V4L2) Firmware
FIRMWARE: Memory map bin file not passed
Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [Location of Mem map bin file]
FIRMWARE: Default memory configuration is used
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.1.1
FIRMWARE: Memory Configuration status : In Progress
FIRMWARE: 2 start Successful
tvp7002 2-005d: tvp7002 found @ 0x5d (OMAP I2C adapter)
tvp7002 2-005d: Rev. 02 detected.
ti81xxvin ti81xxvin: registered sub device tvp7002
ti81xxvin ti81xxvin: TI81xx HDVPSS Capture driver initialized
HDMI W1 rev 2.0
Timing Info:
pixel_clk = 148500
x_res = 1920
y_res = 1080
hfp = 88
hsw = 44
hbp = 148
vfp = 4
vsw = 5
vbp = 36
chown: unknown user messagebus
5.04
SysLink version : 2.10.03.20
SysLink module created on Date:Apr 29 2012 Time:20:45:11
FIRMWARE: I2cInit will be done by M3
FIRMWARE: Memory map bin file not passed
Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [-mmap <memory_map_file>] [-i2c <0|1>]
===Mandatory arguments===
<Processor Id> 0: DSP, 1: Video-M3, 2: Vpss-M3
<Location of Firmware> firmware binary file
<start|stop> to start/stop the firmware
===Optional arguments===
-mmap input memory map bin file name
-i2c 0: i2c init not done by M3, 1(default): i2c init done by M3
FIRMWARE: isI2cInitRequiredOnM3: 1
FIRMWARE: Default memory configuration is used
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.2.1
FIRMWARE: Memory Configuration status : In Progress
FIRMWARE: 1 start Successful
Loading HDVPSS (V4L2) Firmware
FIRMWARE: I2cInit will be done by M3
FIRMWARE: Memory map bin file not passed
Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [-mmap <memory_map_file>] [-i2c <0|1>]
===Mandatory arguments===
<Processor Id> 0: DSP, 1: Video-M3, 2: Vpss-M3
<Location of Firmware> firmware binary file
<start|stop> to start/stop the firmware
===Optional arguments===
-mmap input memory map bin file name
-i2c 0: i2c init not done by M3, 1(default): i2c init done by M3
FIRMWARE: isI2cInitRequiredOnM3: 1
FIRMWARE: Default memory configuration is used
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.2.1
FIRMWARE: Memory Configuration status : In Progress
FIRMWARE: 2 start Successful
tvp7002 2-005d: tvp7002 found @ 0x5d (OMAP I2C adapter)
omap_i2c omap_i2c.2: controller timed out
omap_i2c omap_i2c.2: controller timed out
omap_i2c omap_i2c.2: controller timed out
omap_i2c omap_i2c.2: controller timed out
omap_i2c omap_i2c.2: controller timed out
tvp7002 2-005d: TVP7002 read error -110
tvp7002: probe of 2-005d failed with error -110
ti81xxvin ti81xxvin: Error registering v4l2 subdevice
HDMI W1 rev 2.0