1) SPRS277C indicates all code requires sprc203 ‘system patch’ and that a minimum of 0x2048 32-bit words are required for the patch.
Does this patch need to be applied to only the code that runs from the initial TI Bootloader? Or to all code? the SecondaryBootloader and application code ?
2) this patch seems to be old and not EABI complicant, is that true ? Would the source be available to recomplie and support C6000 EABI ?