This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Filesystem issue with WEC7

Hello,

I just noticed one issue with Filesystem with WEC7.

The board is Mistral REV G.

BSP is BSP_WINCE_ARM_A8_02_00_00.

The catalog items selected are:

Binary Rom Image File System

exFAT File System

FAT File System

Partition Driver

Release Directory File System

Transaction-Safe FAT File System

The problem is the following:

1. low-level format NAND flash in eboot and boot the OS.

2. Select "properties" of "Mounted Volume".

    It shows the following information:

    Used: 16KB

    Free:  424MB

3. Copy some files to "Mounted Volume".

4. Browse "Mounted Volume" folder, all the files are copied.

5. Select "properties" of "Mounted Volume".

    It shows the following information:

    Used: 66.5MB

    Free:  357.5MB

    Everything is fine so far.

6. power cycle the EVM

7. Select "properties" of "Mounted Volume".

    It shows the following information:

    Used: 16KB

    Free:  424MB

8. Browse "Mounted Volume" folder, all the files exist.

The problem here is "Properties" does show the correct information after the reset.

I did the same test with CE6 and CE6 has no problem.

Have you guys encountered the similar issue?

Any insights are appreciated.

Regards,

James