This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

gstreamer-ti_svnr962 DM368 build problem



When I try to build gstreamer I got error message:

cc1: warning: /home/rd/ti_dvsdk/linux-devkit//arm-none-linux-gnueabi/home/rd/DaVinci/rootfs/usr/include/glib-2.0:

It looks like it connect together two include path. I think it reather should looks like

/home/rd/DaVinci/rootfs/usr/include/glib-2.0

Then I got error:

In file included from ../gstregistry.h:28,
                 from ../gst_private.h:42,
                 from parse.l:2:
../../gst/gstplugin.h:32:21: error: gmodule.h: No such file or directory

it is followed by lot of errors, but the major problem I suppose is wrong configuration

I have checked and this file exist in my target library folder.

It looks like it take wrong path to glib, which has been build succesfully. When I mannualy configure and compile gstreamer-0.10.30 it looks allright. Anyone knows where is problem there?

It is very inconvenient to build whole module separately when there is makefile for build all of them.

I use dvsdk4.02 and DM368 SOC

Thanks in advance!