Hi there,
I just installed the new EZSDK5.04 release. I haven't touch anything yet.
I did a simple reboot after I set up u-boot environment variable
using the default *.minicom file. Although the board was booted
into Linux, It failed to load all other drivers.
root@dm816x-evm:~# lsmod
Module Size Used by
syslink 1119122 0
ipv6 209855 12
My investigation shows that the loading of vpss
driver failed. I assume "sbufaddr=0xBF000000"
is correct for this build. I was using "sbufaddr=0xA0200000"
in 5.03 before. I also tried the old address when inserting
vpss.ko but It didn't fix the issue.
Thanks,
-Perry
============================================================================
NET: Registered protocol family 10
ALSA: Restoring mixer settings...
NOT configuring network interfaces: / is an NFS mount
No state is present for card EVM
Found hardware: "" "" "" "" ""
Hardware is initialized using a generic method
No state is present for card EVM
Sun Apr 29 22:50:00 UTC 2012
INIT: Entering runlevel: 5
Loading HDVICP2 Firmware
DM816X prcm_config_app version: 2.0.0.1
Doing PRCM settings...
PRCM for IVHD0 is in Progress, Please wait.....
BW Phy Addr : 0x48180600 Data : 0x00000002
AW Phy Addr : 0x48180600 Data : 0x00000002
Phy Addr : 0x48180c04 Data : 0x00000037
BW Phy Addr : 0x48180620 Data : 0x00070000
AW Phy Addr : 0x48180620 Data : 0x00070002
BW Phy Addr : 0x48180624 Data : 0x00030000
AW Phy Addr : 0x48180624 Data : 0x00010002
Phy Addr : 0x48180600 Data : 0x00000102
BW Phy Addr : 0x48180c10 Data : 0x00000007
AW Phy Addr : 0x48180c10 Data : 0x00000003
Phy Addr : 0x48180c14 Data : 0x00000004
BW Phy Addr : 0x58088000 Data : 0x02dd0aa5
AW Phy Addr : 0x58088000 Data : 0xeafffffe
BW Phy Addr : 0x58098000 Data : 0x480883e2
AW Phy Addr : 0x58098000 Data : 0xeafffffe
BW Phy Addr : 0x48180c10 Data : 0x00000003
AW Phy Addr : 0x48180c10 Data : 0x00000000
Phy Addr : 0x48180c14 Data : 0x00000007
PRCM for IVHD0 is Done Successfully
PRCM for IVHD1 is in Progress, Please wait.....
BW Phy Addr : 0x48180700 Data : 0x00000002
AW Phy Addr : 0x48180700 Data : 0x00000002
Phy Addr : 0x48180d04 Data : 0x00000037
BW Phy Addr : 0x48180720 Data : 0x00070000
AW Phy Addr : 0x48180720 Data : 0x00050002
BW Phy Addr : 0x48180724 Data : 0x00030000
AW Phy Addr : 0x48180724 Data : 0x00010002
Phy Addr : 0x48180700 Data : 0x00000102
BW Phy Addr : 0x48180d10 Data : 0x00000007
AW Phy Addr : 0x48180d10 Data : 0x00000003
Phy Addr : 0x48180d14 Data : 0x00000004
BW Phy Addr : 0x5a088000 Data : 0xafae1ea4
AW Phy Addr : 0x5a088000 Data : 0xeafffffe
BW Phy Addr : 0x5a098000 Data : 0x60aaed4c
AW Phy Addr : 0x5a098000 Data : 0xeafffffe
BW Phy Addr : 0x48180d10 Data : 0x00000003
AW Phy Addr : 0x48180d10 Data : 0x00000000
Phy Addr : 0x48180d14 Data : 0x00000007
PRCM for IVHD1 is Done Successfully
PRCM for IVHD2 is in Progress, Please wait.....
BW Phy Addr : 0x48180800 Data : 0x00000002
AW Phy Addr : 0x48180800 Data : 0x00000002
Phy Addr : 0x48180e04 Data : 0x00000037
BW Phy Addr : 0x48180820 Data : 0x00070000
AW Phy Addr : 0x48180820 Data : 0x00050002
BW Phy Addr : 0x48180824 Data : 0x00030000
AW Phy Addr : 0x48180824 Data : 0x00010002
Phy Addr : 0x48180800 Data : 0x00000102
BW Phy Addr : 0x48180e10 Data : 0x00000007
AW Phy Addr : 0x48180e10 Data : 0x00000003
Phy Addr : 0x48180e14 Data : 0x00000004
BW Phy Addr : 0x53088000 Data : 0x38ebe6ff
AW Phy Addr : 0x53088000 Data : 0xeafffffe
BW Phy Addr : 0x53098000 Data : 0xab40921f
AW Phy Addr : 0x53098000 Data : 0xeafffffe
BW Phy Addr : 0x48180e10 Data : 0x00000003
AW Phy Addr : 0x48180e10 Data : 0x00000000
Phy Addr : 0x48180e14 Data : 0x00000007
PRCM for IVHD2 is Done Successfully
PRCM Initialization completed
SysLink version : 2.10.03.20
SysLink module created on Date:Apr 29 2012 Time:20:45:11
FIRMWARE: I2cInit will be done by M3
FIRMWARE: Memory map bin file not passed
Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [-mmap <memory_map_file>] [-i2c <0|1>]
===Mandatory arguments===
<Processor Id> 0: DSP, 1: Video-M3, 2: Vpss-M3
<Location of Firmware> firmware binary file
<start|stop> to start/stop the firmware
===Optional arguments===
-mmap input memory map bin file name
-i2c 0: i2c init not done by M3, 1(default): i2c init done by M3
FIRMWARE: isI2cInitRequiredOnM3: 1
FIRMWARE: Default memory configuration is used
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.2.1
FIRMWARE: Memory Configuration status : In Progress
FIRMWARE: 1 start Successful
Loading HDVPSS Firmware
FIRMWARE: I2cInit will be done by M3
FIRMWARE: Memory map bin file not passed
Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [-mmap <memory_map_file>] [-i2c <0|1>]
===Mandatory arguments===
<Processor Id> 0: DSP, 1: Video-M3, 2: Vpss-M3
<Location of Firmware> firmware binary file
<start|stop> to start/stop the firmware
===Optional arguments===
-mmap input memory map bin file name
-i2c 0: i2c init not done by M3, 1(default): i2c init done by M3
FIRMWARE: isI2cInitRequiredOnM3: 1
FIRMWARE: Default memory configuration is used
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.2.1
FIRMWARE: Memory Configuration status : In Progress
FIRMWARE: 2 start Successful
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
VPSS_CORE : Failed to init fvid2 interface,
vpss: probe of vpss failed with error -22
VPSS_CORE : failed to register ti81xx-vpss driver
FATAL: Error inserting vpss (/lib/modules/2.6.37/kernel/drivers/video/ti81xx/vpss/vpss.ko): No such device
BUG: Your driver calls ioremap() on system memory. This leads
to architecturally unpredictable behaviour on ARMv6+, and ioremap()
will fail in the next kernel release. Please fix your driver.
------------[ cut here ]------------
WARNING: at arch/arm/mm/ioremap.c:211 __arm_ioremap_pfn_caller+0x58/0x190()
Modules linked in: vpss(+) syslink ipv6
Backtrace:
[<c0049bb8>] (dump_backtrace+0x0/0x110) from [<c039b7d4>] (dump_stack+0x18/0x1c)
r7:00000000 r6:c004d76c r5:c045bf9b r4:000000d3
[<c039b7bc>] (dump_stack+0x0/0x1c) from [<c006da3c>] (warn_slowpath_common+0x54/0x6c)
[<c006d9e8>] (warn_slowpath_common+0x0/0x6c) from [<c006da78>] (warn_slowpath_null+0x24/0x2c)
r9:ef3a0000 r8:c04eee88 r7:bf1c5530 r6:000a0200 r5:00200000
r4:00000000
[<c006da54>] (warn_slowpath_null+0x0/0x2c) from [<c004d76c>] (__arm_ioremap_pfn_caller+0x58/0x190)
[<c004d714>] (__arm_ioremap_pfn_caller+0x0/0x190) from [<c004d928>] (__arm_ioremap_caller+0x64/0x6c)
[<c004d8c4>] (__arm_ioremap_caller+0x0/0x6c) from [<c0060454>] (omap_ioremap+0x60/0x64)
r6:00000000 r5:00200000 r4:a0200000
[<c00603f4>] (omap_ioremap+0x0/0x64) from [<bf1c5530>] (vps_sbuf_init+0x108/0x1c0 [vpss])
r7:bf1be628 r6:00200000 r5:a0200000 r4:eed96ec0
[<bf1c5428>] (vps_sbuf_init+0x0/0x1c0 [vpss]) from [<bf1af0b0>] (vps_probe+0x4c/0x174 [vpss])
r8:c0506ed0 r7:ef3fdc80 r6:bf1be5c0 r5:c04eee90 r4:c04eee88
[<bf1af064>] (vps_probe+0x0/0x174 [vpss]) from [<c02047b0>] (platform_drv_probe+0x20/0x24)
r7:ef3fdc80 r6:bf1be12c r5:c04eee90 r4:c04eee90
[<c0204790>] (platform_drv_probe+0x0/0x24) from [<c020371c>] (driver_probe_device+0xd0/0x190)
[<c020364c>] (driver_probe_device+0x0/0x190) from [<c0203844>] (__driver_attach+0x68/0x8c)
r7:ef3fdc80 r6:bf1be12c r5:c04eeec4 r4:c04eee90
[<c02037dc>] (__driver_attach+0x0/0x8c) from [<c0202ec8>] (bus_for_each_dev+0x50/0x84)
r7:ef3fdc80 r6:bf1be12c r5:c02037dc r4:00000000
[<c0202e78>] (bus_for_each_dev+0x0/0x84) from [<c0203540>] (driver_attach+0x20/0x28)
r6:bf1be12c r5:bf1be118 r4:00000000
[<c0203520>] (driver_attach+0x0/0x28) from [<c02027a0>] (bus_add_driver+0xb4/0x234)
[<c02026ec>] (bus_add_driver+0x0/0x234) from [<c0203b7c>] (driver_register+0xb0/0x13c)
[<c0203acc>] (driver_register+0x0/0x13c) from [<c0204a9c>] (platform_driver_register+0x4c/0x60)
r9:ef3a0000 r8:bf1c4000 r7:400ee000 r6:0001b218 r5:bf1be118
r4:00000000
[<c0204a50>] (platform_driver_register+0x0/0x60) from [<c0204ad0>] (platform_driver_probe+0x20/0x70)
[<c0204ab0>] (platform_driver_probe+0x0/0x70) from [<bf1c4030>] (vps_init+0x30/0x5c [vpss])
r5:bf1be49c r4:00000000
[<bf1c4000>] (vps_init+0x0/0x5c [vpss]) from [<c003b42c>] (do_one_initcall+0xd0/0x1a4)
[<c003b35c>] (do_one_initcall+0x0/0x1a4) from [<c0099158>] (sys_init_module+0x9c/0x1bc)
[<c00990bc>] (sys_init_module+0x0/0x1bc) from [<c0045e00>] (ret_fast_syscall+0x0/0x30)
r7:00000080 r6:00000000 r5:0001b218 r4:400dabe0
---[ end trace 4bd8f4fc586b05f5 ]---
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
VPSS_CORE : Failed to init fvid2 interface,
vpss: probe of vpss failed with error -22
VPSS_CORE : failed to register ti81xx-vpss driver
FATAL: Error inserting ti81xxfb (/lib/modules/2.6.37/kernel/drivers/video/ti81xx/ti81xxfb/ti81xxfb.ko): No such device
open /dev/fb0: No such file or directory
BUG: Your driver calls ioremap() on system memory. This leads
to architecturally unpredictable behaviour on ARMv6+, and ioremap()
will fail in the next kernel release. Please fix your driver.
------------[ cut here ]------------
WARNING: at arch/arm/mm/ioremap.c:211 __arm_ioremap_pfn_caller+0x58/0x190()
Modules linked in: vpss(+) syslink ipv6
Backtrace:
[<c0049bb8>] (dump_backtrace+0x0/0x110) from [<c039b7d4>] (dump_stack+0x18/0x1c)
r7:00000000 r6:c004d76c r5:c045bf9b r4:000000d3
[<c039b7bc>] (dump_stack+0x0/0x1c) from [<c006da3c>] (warn_slowpath_common+0x54/0x6c)
[<c006d9e8>] (warn_slowpath_common+0x0/0x6c) from [<c006da78>] (warn_slowpath_null+0x24/0x2c)
r9:eee6a000 r8:c04eee88 r7:bf1e5530 r6:000a0200 r5:00200000
r4:00000000
[<c006da54>] (warn_slowpath_null+0x0/0x2c) from [<c004d76c>] (__arm_ioremap_pfn_caller+0x58/0x190)
[<c004d714>] (__arm_ioremap_pfn_caller+0x0/0x190) from [<c004d928>] (__arm_ioremap_caller+0x64/0x6c)
[<c004d8c4>] (__arm_ioremap_caller+0x0/0x6c) from [<c0060454>] (omap_ioremap+0x60/0x64)
r6:00000000 r5:00200000 r4:a0200000
[<c00603f4>] (omap_ioremap+0x0/0x64) from [<bf1e5530>] (vps_sbuf_init+0x108/0x1c0 [vpss])
r7:bf1de628 r6:00200000 r5:a0200000 r4:eed96b80
[<bf1e5428>] (vps_sbuf_init+0x0/0x1c0 [vpss]) from [<bf1cf0b0>] (vps_probe+0x4c/0x174 [vpss])
r8:c0506ed0 r7:ef3fda00 r6:bf1de5c0 r5:c04eee90 r4:c04eee88
[<bf1cf064>] (vps_probe+0x0/0x174 [vpss]) from [<c02047b0>] (platform_drv_probe+0x20/0x24)
r7:ef3fda00 r6:bf1de12c r5:c04eee90 r4:c04eee90
[<c0204790>] (platform_drv_probe+0x0/0x24) from [<c020371c>] (driver_probe_device+0xd0/0x190)
[<c020364c>] (driver_probe_device+0x0/0x190) from [<c0203844>] (__driver_attach+0x68/0x8c)
r7:ef3fda00 r6:bf1de12c r5:c04eeec4 r4:c04eee90
[<c02037dc>] (__driver_attach+0x0/0x8c) from [<c0202ec8>] (bus_for_each_dev+0x50/0x84)
r7:ef3fda00 r6:bf1de12c r5:c02037dc r4:00000000
[<c0202e78>] (bus_for_each_dev+0x0/0x84) from [<c0203540>] (driver_attach+0x20/0x28)
r6:bf1de12c r5:bf1de118 r4:00000000
[<c0203520>] (driver_attach+0x0/0x28) from [<c02027a0>] (bus_add_driver+0xb4/0x234)
[<c02026ec>] (bus_add_driver+0x0/0x234) from [<c0203b7c>] (driver_register+0xb0/0x13c)
[<c0203acc>] (driver_register+0x0/0x13c) from [<c0204a9c>] (platform_driver_register+0x4c/0x60)
r9:eee6a000 r8:bf1e4000 r7:400c9000 r6:0001b208 r5:bf1de118
r4:00000000
[<c0204a50>] (platform_driver_register+0x0/0x60) from [<c0204ad0>] (platform_driver_probe+0x20/0x70)
[<c0204ab0>] (platform_driver_probe+0x0/0x70) from [<bf1e4030>] (vps_init+0x30/0x5c [vpss])
r5:bf1de49c r4:00000000
[<bf1e4000>] (vps_init+0x0/0x5c [vpss]) from [<c003b42c>] (do_one_initcall+0xd0/0x1a4)
[<c003b35c>] (do_one_initcall+0x0/0x1a4) from [<c0099158>] (sys_init_module+0x9c/0x1bc)
[<c00990bc>] (sys_init_module+0x0/0x1bc) from [<c0045e00>] (ret_fast_syscall+0x0/0x30)
r7:00000080 r6:00000000 r5:0001b208 r4:400fabe0
---[ end trace 4bd8f4fc586b05f6 ]---
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
notify_shm_drv_sendevent failed! status = 0xfffffff0
notify_send_event failed! status = 0xfffffff0
VPSS_CORE : Failed to init fvid2 interface,
vpss: probe of vpss failed with error -22
VPSS_CORE : failed to register ti81xx-vpss driver
FATAL: Error inserting ti81xxhdmi (/lib/modules/2.6.37/kernel/drivers/video/ti81xx/ti81xxhdmi/ti81xxhdmi.ko): No such device
Starting system message bus: dbus.
Starting telnet daemon.
Starting syslogd/klogd: done
Starting thttpd.
Starting Matrix GUI application.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org dm816x-evm ttyO2
Arago 2011.09 dm816x-evm ttyO2
dm816x-evm login: root
root@dm816x-evm:~# lsmod
Module Size Used by
syslink 1119122 0
ipv6 209855 12
root@dm816x-evm:~#