This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Help, DM8168 EZSDK

hi, all

I made an 8168 EVM board according to Spectrum Digital's DM816x Evaluation Module(reversion G), but when power up, the uart2  print nothing, the power sequence goes fine, the board is confugured to boot from SD card(I format the sd card by ti-ezsdk_dm816x-evm_5_03_01_15 tools), and I am sure the configure switch setting is all right, but the uart2 just print nothing....the board I made does not contain the EEPROM whitch hold the board version information, is this OK? would EZSDK linux demo run successfully without the EEPROM?

hope help

qing