This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Decoding and Encoding capabilities issue/question in EVM8168 , SDK 5.04



Hi,

We are using following OMX application pipeline : File(1080p30)->VDEC->DEI(1080p30)->Display

                                                                                                                             |_VENC

We have 2 such pipelines running simultanesly so in total we have : 2 1080p30 Decode and 2 Encode. 

The problem is that in Encoding we can only use 480p30 resolution , if we try 720p30 the VENC component will not transfer to Idle state.

The exactly same code works fine with 480p30 resolution.

So the question is where is the limitation ? in OMX implementation ? in Ducati code ?

Form the hardware spec we understand there is 3 HDVICP units which should be enough to handle these loads.

Please Advise,

Vladik