The page below
http://processors.wiki.ti.com/index.php/SysLink_MMU_Support
indicates that MMU is turned off for the DSP when using syslink 2.10 and later. How does one verify that ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The page below
http://processors.wiki.ti.com/index.php/SysLink_MMU_Support
indicates that MMU is turned off for the DSP when using syslink 2.10 and later. How does one verify that ?
If you don't want to trust the documentation, you can try to check the MMU registers to see if it is enabled. I think there is an MMUENABLE bit in the MMU_CNTL register which should be 0 to ensure the MMU is off. Please refer to the device's TRM documentation for more information on the MMU registers.
Best regards,
Vincent
Thanks for your response. I am looking at the TRM (Literature Number: SPRUGZ8A 14 November 2011–Revised February 2012) section 1.4.5 (MMU Registers) and I don't see a definition for the base address of the MMU. All registers are listed in terms of offsets. I must be missing something rather basic here?
Andrew Elder said:Thanks for your response. I am looking at the TRM (Literature Number: SPRUGZ8A 14 November 2011–Revised February 2012) section 1.4.5 (MMU Registers) and I don't see a definition for the base address of the MMU. All registers are listed in terms of offsets. I must be missing something rather basic here?
I also checked the datasheet sprs647c.pdf.
In the datasheet, page 30, there is an entry for 'DEMMU Peripheral Registers'. I think that is what you are looking for. You may also want to check with the device forum if you need additional details.
Best regards,
-Vincent