This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Android upper always restart



Hi,all
   In the input subsystem, I add another reader thread .Implementation method is the same as InputReaderThread.
   After that, android upper always restart.
   Does anyone known why?

  • Hi Yanhong,

    1. Are you adding a support for new input device ? if yes, then do  - "$getevent -p" on console and see if your device is getting listed there.

    2. What are you trying to achieve in new reader thread - could you clarify more on that ?

    3. Few observations from log...

    01-01 00:46:00.179: DEBUG/Button Savior(5044): admin api detecting
    01-01 00:46:00.351: DEBUG/Button savir(5044): su not found

    Are you trying to run something with su permission ??

    in case if you are doing any thing with brightness ? then give proper permission to below node in init.rc file

    write_int failed to open /dev/brightness

    BR,

    satish

  • Hi satish,

    I want to add the function of the serial keys. Therefore, I add a reader thread, read the serial port to get the scan code, and then distribute.
    Now I just define a thread class, and then create a variable, it appears the restart phenomenon.
    I add the following contents:

    (1)================Define the thread class  InputReaderThread2===============
    file:InputReader.h
    291 /* Reads raw events from the event hub and processes them, endlessly. */
     292 class InputReaderThread : public Thread {
     293 public:
     294     InputReaderThread(const sp<InputReaderInterface>& reader);
     295     virtual ~InputReaderThread();
     296
     297 private:
     298     sp<InputReaderInterface> mReader;
     299
     300     virtual bool threadLoop();
     301 };
     302 /**************************add start*********************/
     303 /* Reads raw events from uart devices  and processes them, endlessly. */
     304 class InputReaderThread2 : public Thread {
     305 public:
     306     InputReaderThread2();
     307     virtual ~InputReaderThread2();
     308
     309 private:
     310     virtual bool threadLoop();
     311 };
     312 /**************************add end*********************/

     (2)================The realization of the functional===============
     file:InputReader.cpp
     627 // --- InputReaderThread ---
     628
     629 InputReaderThread::InputReaderThread(const sp<InputReaderInterface>& reader) :
     630         Thread(/*canCallJava*/ true), mReader(reader) {
     631 }
     632
     633 InputReaderThread::~InputReaderThread() {
     634 }
     635
     636 bool InputReaderThread::threadLoop() {
     637     mReader->loopOnce();
     638     return true;
     639 }
     640 /**************************add start*********************/
     641 // --- InputReaderThread2 ---
     642
     643 InputReaderThread2::InputReaderThread2() :
     644         Thread(/*canCallJava*/ true) {
     645 }
     646
     647 InputReaderThread2::~InputReaderThread2() {
     648 }
     649
     650 bool InputReaderThread2::threadLoop() {
     651     return true;
     652 }
     653/**************************add end*********************/

     (3))=================Define the class variable==============
      file:InputManager.h
      class:InputManager
      105 private:
      106     sp<InputReaderInterface> mReader;
      107     sp<InputReaderThread> mReaderThread;
      108     /**************************add start*********************/
      109     sp<InputReaderThread2> mReaderThread2;
      110     /**************************add end*********************/
      111     sp<InputDispatcherInterface> mDispatcher;
      112     sp<InputDispatcherThread> mDispatcherThread;
        
        It appears the restart phenomenon after adding these.

        Now,it works well when I add "setprop libc.debug.malloc 10" to init.rc.But I do not know why.

  • Hi,

    I am not sure but you need to relook your code for some kind of memory leak. As property you have mentioned is to be set when we debug memory

    http://source.android.com/tech/debugging/native-memory.html

    Also, you can refer to

    http://code.google.com/p/android-serialport-api/

    for serial port access

     

    BR,

    satish

  • yanhong wu said:

    I want to add the function of the serial keys. Therefore, I add a reader thread, read the serial port to get the scan code, and then distribute.
    Now I just define a thread class, and then create a variable, it appears the restart phenomenon.

    An alternate approach you can explore is to implement a kernel driver for the serial keys. This way android will see this a normal input device and you need not modify the android frameworks.

  • Hi Vishveshwar,

    I think that what you said is a good method, but I do not know how to operate the serial device in the kernel.Can you give me some guidance or some examples?

    In addition, after a few restarts, it is no longer reboot and run well.I suspect that android reboot is due to insufficient memory.Can you give me some suggestions on how to debug?

  • The latest test found that adding an integer variable in InputManger class also causes the android upper restart

    eg:
    TI_Android_GingerBread_2_3_4Sources/frameworks/base/include/ui/InputManager.h

     84 class InputManager : public InputManagerInterface {
     85 protected:
     86     virtual ~InputManager();
     87
     88 public:
     89     InputManager(
     90             const sp<EventHubInterface>& eventHub,
     91             const sp<InputReaderPolicyInterface>& readerPolicy,
     92             const sp<InputDispatcherPolicyInterface>& dispatcherPolicy);
     93
     94     // (used for testing purposes)
     95     InputManager(
     96             const sp<InputReaderInterface>& reader,
     97             const sp<InputDispatcherInterface>& dispatcher);
     98
     99     virtual status_t start();
    100     virtual status_t stop();
    101
    102     virtual sp<InputReaderInterface> getReader();
    103     virtual sp<InputDispatcherInterface> getDispatcher();
    104
    105 private:
    106     sp<InputReaderInterface> mReader;
    107     sp<InputReaderThread> mReaderThread;
    108     /***********add start********/
    109     int abc;
    110     /************add end*********/
    111     sp<InputDispatcherInterface> mDispatcher;
    112     sp<InputDispatcherThread> mDispatcherThread;
    113
    114     void initialize();
    115 };