This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SDRAM Timing 3 Register

 Hi DM8168 champs!!

The "Technical Reference Manual SPRUGX8-1 July 2011 - Tables 7-32 and 7-44 SDRAM Timing 3 Register" show that T_RASMAX must be programmed to Fh. The spread sheet "C6A8168 DDR calculate sheet", gives the value 8 instead. What is the reason to program Fh for that parameter? Also, "Table 7-33 DDR PHY Control Register" shows that RL is programmed to Max RL (CAS latency + 7 -1 = 17). Could this cause a timing problem if this field is programmed to a lower value (CAS +1 -1 = 11 for example)?

Thanks!

 Anjli