Hi
I am Using TSC2007 Touch Screen IC used to interface LCD and DM8148 Via I2C
I am facing following issues when interfaced TSC2007 with DM814X
1.Not all the time the I2C address is detected. Problem occurs if Power ON/OFF cycle carried out immediately (2sec to 3Sec maintained atleast).
2.SDA goes low when LCD touch screen is touch continuously or it is touched multiple time. (If delay programmed is less than 1ms to read the activity)
3.After device lock up (SDA goes low), device is not recovering to its actual state even after providing I2C reset using SCL from master.
4.TSC2007 (Slave) recovers only after Power cycle.
I have read the TI Application Report for TSC2007 SBAA161–March2009 (Important Considerations to Assure a Safe POR) and i came up with conclusin that above issues are because of Silicon issue related to the device.Correct me if i am wrong.
Also please suggest me if there is any alternate available to overcome above issues.
Regards
Kinjan