Hi,
I am trying to run the ipnc application on DM368IPNC board on Appro design
but the image sensor board from some other vendor.Sometimes it works fine
that we are able to see the camera display but we get the following message in log.
ChipX id fail.Please contact appropho.com.
Lately now in same set up the boot process hangs unexpectedly.Boot log is as follows:
DM368 IPNC :>
DM36x initialization passed!
TI UBL Base Version: 1.50
Boot Loader BootMode = NAND
Starting NAND Copy...
Valid magicnum, 0xA1ACED66, found in block 0x00000008.
Boot Mode Task Completed
IPNC UBL Version: 1.1.0
Platform: DM368
Jumping to entry point at 0x81080000
U-Boot 1.3.4 (Dec 9 2010 - 17:44:14) DM368-IPNC-1.0.1
I2C: ready
DRAM: 128 MB
NAND: NAND device: Manufacturer ID: 0xec, Chip ID: 0xf1 (Samsung NAND 128MiB 3,3V 8-bit)
Bad block table found at page 65472, version 0x01
Bad block table found at page 65408, version 0x01
128 MiB
In: serial
Out: serial
Err: serial
ARM Clock :- 432MHz
DDR Clock :- 340MHz
Ethernet PHY: GENERIC @ 0x01
Hit any key to stop autoboot: 0
NAND read: device 0 offset 0x700000, size 0xe00000
Skipping bad block 0x00b80000
14680064 bytes read: OK
Loading from NAND 128MiB 3,3V 8-bit, offset 0x500000
Image Name: Linux-2.6.18_pro500-davinci_IPNC
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1883832 Bytes = 1.8 MB
Load Address: 80008000
Entry Point: 80008000
## Booting kernel from Legacy Image at 80700000 ...
Image Name: Linux-2.6.18_pro500-davinci_IPNC
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1883832 Bytes = 1.8 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Linux version 2.6.18_pro500-davinci_IPNC_DM368_2.6.0 (root@mayank-a) (gcc version 4.2.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #1 PREEMPT Tue May 8 16:55:43 IS2
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
Machine: DaVinci DM368 IPNC
Memory policy: ECC disabled, Data cache writeback
DaVinci DM0365 variant 0x8
PLL0: fixedrate: 24000000, commonrate: 170000000, vpssrate: 340000000
PLL0: vencrate_sd: 75555555, ddrrate: 340000000 mmcsdrate: 48571428
PLL1: armrate: 432000000, voicerate: 20571428, vencrate_hd: 27000000
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Built 1 zonelists. Total pages: 12288
Kernel command line: console=ttyS1,115200n8 noinitrd rw ip=192.168.1.1:192.168.1.50:255.255.255.0 root=/dev/nfs nfsroot=192.168.1.50:/home/mayank/DM368IPCM/ipnc/targetM
PID hash table entries: 256 (order: 8, 1024 bytes)
Clock event device timer0_0 configured with caps set: 07
Console: colour dummy device 80x30
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory: 48MB = 48MB total
Memory: 44544KB available (3229K code, 658K data, 184K init)
Security Framework v1.0.0 initialized
Capability LSM initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
NET: Registered protocol family 16
DaVinci: 104 gpio irqs
MUX: initialized GPIO20
MUX: initialized I2C_SCL
Generic PHY: Registered new driver
ch0 default output "COMPOSITE", mode "NTSC"
VPBE Encoder Initialized
SCSI subsystem initialized
NET: Registered protocol family 2
IP route cache hash table entries: 512 (order: -1, 2048 bytes)
TCP established hash table entries: 2048 (order: 1, 8192 bytes)
TCP bind hash table entries: 1024 (order: 0, 4096 bytes)
TCP: Hash tables configured (established 2048 bind 1024)
TCP reno registered
***davinci_spi_board_init()!<6>
***davinci_spi_board_init_End(0)!<5>VFS: Disk quotas dquot_6.5.1
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
squashfs: version 3.1 (2006/08/19) Phillip Lougher
JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.
yaffs May 8 2012 16:53:52 Installing.
SGI XFS with no debug enabled
Initializing Cryptographic API
io scheduler noop registered
io scheduler anticipatory registered (default)
LTT : ltt-facilities init
LTT : ltt-facility-core init in kernel
DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec
Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfbc20000 (irq = 40) is a 16550A
serial8250.0: ttyS1 at MMIO map 0x1d06000 mem 0xfbd06000 (irq = 41) is a 16550A
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
Davinci EMAC MII Bus: probed
MAC address is deadbeaf
TI DaVinci EMAC Linux version updated 4.0
netconsole: not configured, aborting
Linux video capture interface: v2.00
Trying to register davinci display video device.
layer=c059e000,layer->video_dev=c059e160
Trying to register davinci display video device.
layer=c0584e00,layer->video_dev=c0584f60
davinci_init:DaVinci V4L2 Display Driver V1.0 loaded
i2c /dev entries driver
Generic platform RAM MTD, (c) 2004 Simtec Electronics
nand_davinci nand_davinci.0: Using 4-bit hardware ECC
NAND device: Manufacturer ID: 0xec, Chip ID: 0xf1 (Samsung NAND 128MiB 3,3V 8-bit)
Creating 7 MTD partitions on "nand_davinci.0":
0x00000000-0x00300000 : "bootloader"
mtd: Giving out device 0 to bootloader
0x00300000-0x00500000 : "params"
mtd: Giving out device 1 to params
0x00500000-0x00700000 : "kernel"
mtd: Giving out device 2 to kernel
0x00700000-0x02700000 : "filesystem"
mtd: Giving out device 3 to filesystem
0x02700000-0x02900000 : "data1"
mtd: Giving out device 4 to data1
0x02900000-0x02d00000 : "Calibration"
mtd: Giving out device 5 to Calibration
0x02d00000-0x08000000 : "data2"
mtd: Giving out device 6 to data2
nand_davinci nand_davinci.0: hardware revision: 2.3
MUX: initialized SPI0_SCLK
MUX: initialized SPI0_SDO)
dm_spi.0: davinci SPI Controller driver at 0xc3866000 (irq = 42) use_dma=0
musb_hdrc: version 6.0, cppi-dma, peripheral, debug=0
musb_hdrc musb_hdrc: No DMA interrupt line
musb_hdrc: USB Peripheral mode controller at c3868000 using DMA, IRQ 12
rtc_davinci_dm365 rtc_davinci_dm365.0: rtc intf: proc
rtc_davinci_dm365 rtc_davinci_dm365.0: rtc intf: dev (254:0)
rtc_davinci_dm365 rtc_davinci_dm365.0: rtc core: registered rtc_davinci_dm365 as rtc0
davinci-mmc davinci-mmc.0: Supporting 4-bit mode
davinci-mmc davinci-mmc.0: Using DMA mode
Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).
ASoC version 0.13.1
CQ0093 Voice Codec 0.1
asoc: cq93vc <-> davinci-vcif mapping ok
ALSA device list:
#0: On-chip voice codec (cq93vc)
IPv4 over IPv4 tunneling driver
TCP bic registered
NET: Registered protocol family 1
NET: Registered protocol family 17
rtc_davinci_dm365 rtc_davinci_dm365.0: setting the system clock to 2000-01-01 01:06:43 (946688803)
Time: timer0_1 clocksource has been installed.
Clock event device timer0_0 configured with caps set: 08
Switched to high resolution mode on CPU 0
IP-Config: Guessing netmask 255.255.255.0
IP-Config: Gateway not on directly connected network.
Looking up port of RPC 100003/2 on 192.168.1.50
Looking up port of RPC 100005/1 on 192.168.1.50
VFS: Mounted root (nfs filesystem).
Freeing init memory: 184K
INIT: version 2.86 booting
0
Starting the hotplug events dispatcher: udevd.
Synthesizing the initial hotplug events...done.
Waiting for /dev to be fully populated...done.
0
CSL: Module install successful, device major num = 253
CSL: Module version 0.10.00, built on May 11 2012 10:21:08
I2C: Module install successful, device major num = 252
DMA: Module install successful, device major num = 251
DRV: Module install successful
DRV: Module built on May 11 2012 10:21:09
DRV: EDMACC.QUEPRI = 00000777
DRV: SYSTEM.MSTPRI0 = 00440022
DRV: SYSTEM.MSTPRI1 = 00000244
DRV: ISP.BCR = 00000002
DRV: SYSTEM.MISC = 00000391
CMEMK module: built on May 11 2012 at 10:20:54
Reference Linux version 2.6.18
File /home/mayank/DM368IPCM/dvsdk_2_10_01_18_v2.6/linuxutils_2_24_03/packages/ti/sdo/linuxutils/cmem/src/module/cmemk.c
allocated heap buffer 0xc4000000 of size 0x5000000
CMEM Range Overlaps Kernel Physical - allowing overlap
CMEM phys_start (0x1000) overlaps kernel (0x80000000 -> 0x83000000)
cmemk initialized
EDMAK module: built on May 11 2012 at 10:20:55
Reference Linux version 2.6.18
File /home/mayank/DM368IPCM/dvsdk_2_10_01_18_v2.6/linuxutils_2_24_03/packages/ti/sdo/linuxutils/edma/src/module/edmak.c
IRQK module: built on May 11 2012 at 10:20:56
Reference Linux version 2.6.18
File /home/mayank/DM368IPCM/dvsdk_2_10_01_18_v2.6/linuxutils_2_24_03/packages/ti/sdo/linuxutils/irq/src/module/irqk.c
irqk initialized
Empty flash at 0x001e2830 ends at 0x001e3000
Empty flash at 0x001fa81c ends at 0x001fb000
JFFS2 notice: (559) read_dnode: node CRC failed on dnode at 0x1fa7d8: read 0xffffffff, calculated 0x20d1c69f
JFFS2 notice: (559) read_dnode: node CRC failed on dnode at 0x1e27ec: read 0xffffffff, calculated 0x60708ecd
Creat queue id:0
queue id:0
Creat queue id:32769
queue id:32769
FileMngThread created
queue id:32769
AlramThread created
Share memory init success
IPNC_DM368_2.6.0 (root@mayank-a) (gcc version 4.2.0 (MontaVista
Creat queue id:65538
queue id:65538
queue id:65538
Creat queue id:98307
queue id:98307
CPU is DM368
DEMOCFG Value : 0
Videocodecmode : 0
Videocodecres : 0
Value of pConfig -> nVideocodecmode by default 0
./av_server.out DM368 NTSC APPRO2A AEWB D1 MPEG4 5000000 VBR AUTO MENUOFF &
Check_device_version : DEVICE VER = 1 !!
Starting mounting local filesystems: mount
AVSERVER UI: Initializing.
none on /dev/shm type tmpfs (rw,size=5M)
none on /var/run type tmpfs (rw)
none on /tmp type tmpfs (rw,sync)
CLK Hz,
ARM Hz = 432000000
DDR Hz = 340000000
VPSS Hz = 340000000
IMCOP Hz = 340000000
Setting up networking ... DRV LDC: GetConfig 0003 0x0
[OSA_FILE ] Reading file [/mnt/nand/IMG_Paramset.bin] ... ERROR
IMAGE TUNE: Paramset File is not available..... Setting DEFAULT parameter
ApproDrvInit: 7
Creat queue id:131076
queue id:131076
CONFIGURING AVSERVER FOR DM368 .....
queue id:65538
############OPEN###########
==========>>>> Start X,Y = 52,18
############reset###########
DavinciDisplay DavinciDisplay.1: Before finishing with S_FMT:
layer.pix_fmt.bytesperline = 640,
layer.pix_fmt.width = 640,
layer.pix_fmt.height = 480,
layer.pix_fmt.sizeimage =460800
############SPI DavinciDisplay DavinciDisplay.1: pixfmt->width = 640,
layer->layer_info.config.line_length= 640
OPEN###########
spi mode: 16
bits per word: 8
max speed: 12000000 Hz (12000 KHz)
############SET REG###########
############OPEN END###########
================> 10, 400, 1735
APPRO Setting Applied
queue id:131076
FR : 0 users registered from exsiting face album
IPNC_DM368_2.6.0 (root@mayank-a) (gcc version 4.2.0 (MontaVista
IPNC AUTO_IRIS = 1 (0:Manual,1:Auto)#####################
APPRO 2A Created
XXXXX IAE_CMD_SET_CONFIG XXXXX
.
222 Aew_Cal_LoadParam: dfc check sum success
(nand offset: 0x00500010, size: 0x0000181c, checksum: 0x00020024)
################DFC ret=0##################
Starting hotplug subsystem:
pci
pci [success]
usb
QualityMode:(Index:0)7
Simple mixer control 'PGA',0
Capabilities: cvolume
Capture channels: Mono
Limits: Capture 0 - 3
Mono: Capture 2 [67%]
Simple mixer control 'Mono DAC',0
Capabilities: pvolume pvolume-joined
Playback channels: Mono
Limits: Playback 0 - 63
Mono: Playback 47 [75%]
SystemInit success
Schedule manager init success
usb [success]
isapnp
isapnp [success]
ide
MTD_open
ide [sucMTD_read
cess]
input MTD_close
############################################################
##### AEWB IPNC_DM368IMX036 formal version for FW2.60.01 20120106. #####
############################################################
XXXXX DRV_imgsSetAgain() Error(0)
~~~ fn: Aew_Cal_LoadAutoIrisParam, start ~~~
~~~ fn: Aew_Cal_LoadAutoIrisParam, nand_addr 0x340000 ~~~
!!! FAIL, Checksum error, Aew_Cal_LoadAutoIrisParam, tmp_chksum 354, iris_chksum 47811, iris_test_val 11513604 !!!
!!!!!! FAIL, autoiris default value 0 !!!!!!
Enable APPRO_DBG Function @@@@@@@@@@@@@@@@@@@@@
--->Chip init PASS
Mode:0,F:0,minST=0,(Gain:7),Q:-1
ND Init
ND:Day
input [success]
scsi
swa
when i run ./av_server.out D1 the capture runs fine but no streaming.
Please help.
Regards,
Mayank