Other Parts Discussed in Thread: DM3730
Hello All,
I am using DM3730 and Android 2.3.4 with ti-dvsdk_dm3730-evm_04_03_00_06.
In landscape mode (default mode on our device i.e. fb rotation is 0) the 720P playback is fine using DSP engine. I can see the smooth video playback on the screen.
I portrait mode (fb rotation is set to 270), the same video playback is seen garbage (pink screen on the overlay window) on screen. If I disable overlay then PSP uses the software renderer and the video playback is fine.
May I know what changes are required to see the proper video in portrait (screen rotation 270) mode. Ideally DSP/overlay engine should read the rotation angle from framebuffer and set the same but if it's not the case then may I know the settings?
Thanks,
-Ninad.