Other Parts Discussed in Thread: AM3359
We currently created a AM3359 based board that has 2 mini PCIe slots connected via usb and configured as hosts with the ID pins pulled down. But since the interface is 3.3v power on mini PCIe there was no vbus to feedback to the chip. the problem is that the when the device is plugged in it is not being recognized. In the current PSP 04.06.07.00 is there a way to enable the USB host functionality without a vbus signal? We do have both ports configured as host in the board.c file.
Thanks,
Ed