Other Parts Discussed in Thread: DM3725
The following questions are for the WEC7 BSP for the DM3725.
- Is there any configuration (e.g. via registry) to adjust playback speed?
- Is there any support for WMV files (WMV9 or VC-1 codec)?
- Is there a way to map more FOURCCs to the codecs, e.g. to map DX50 to the MPEG4 video codec or MP4A to AAC audio codec?
- Where is the newest DVSDK (1.11.00.03 I believe) source code for CE6 and/or WEC7 (not the binary only distribution with the CE6 or WEC7 EVM BSPs)?