This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Mcbsp omap3703

Hi,

Iam using omap3703. Mcbsp is used as a slave, with external clock as the source.

I am trying to send the data via mcbsp to audio codec using pcm test program. DMA is triggered and it sends only 2 bytes of data..but i dont see any activity on the pins(i.e, i dont see any clkx or data being pushed out). Anyone has any input on this.

Thanks in Advance..

  • Register dump omap_mcbsp_start...

    [  183.744537] ***********omap_mcbsp_start
    [  183.791809] **** McBSP1 regs **** Begin of this function.
    [  183.831756] DRR2:  0x5527087e
    [  183.867462] DRR1:  0x0000
    [  183.898986] DXR2:  0x0000
    [  183.930511] DXR1:  0x0000
    [  183.962036] SPCR2: 0x0230
    [  183.993560] SPCR1: 0x0030
    [  184.025085] RCR2:  0x8041
    [  184.056610] RCR1:  0x0040
    [  184.088134] XCR2:  0x8041
    [  184.119659] XCR1:  0x0040
    [  184.151184] SRGR2: 0x001f
    [  184.182678] SRGR1: 0x0f00
    [  184.214202] PCR0:  0x000c
    [  184.245727] ***********************

    End of this function.
    [  184.852355] **** McBSP1 regs ****
    [  184.892303] DRR2:  0x5527087e
    [  184.928009] DRR1:  0x0000
    [  184.959533] DXR2:  0x0000
    [  184.991058] DXR1:  0x0000
    [  185.022583] SPCR2: 0x02f5
    [  185.054107] SPCR1: 0x0030
    [  185.085632] RCR2:  0x8041
    [  185.117156] RCR1:  0x0040
    [  185.148651] XCR2:  0x8041
    [  185.180175] XCR1:  0x0040
    [  185.211700] SRGR2: 0x001f
    [  185.243225] SRGR1: 0x0f00
    [  185.274749] PCR0:  0x000c
    [  185.306274] ***********************