This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

using both RTDX and SRIO on EVMC6474

HI everybody!.

I work with ccs3.3 for evmc6474 emulator.

I have a question .please support me.

Can We use both RTDX and SRIO to transfer data between two core on evmc6474?

thank to all of you !

  • tho,

    RTDX is not meant to be used to transfer data between 2 cores.

    RTDX is meant to send data from the target (c6474) to the host (Windows machine).  Now can it actually be used to transfer data between different cores...I don't think so because I've never heard or seen anyone try to do that.

    Judah